<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32Kのトピックs32k144 flexCAN MB</title>
    <link>https://community.nxp.com/t5/S32K/s32k144-flexCAN-MB/m-p/1209189#M9536</link>
    <description>&lt;P&gt;I have a question.&lt;BR /&gt;How is the FLEXCAN_DRV_Receive function configured to receive multiple IDs?&lt;BR /&gt;The FLEXCAN_DRV_ConfigTxMb function is configured to accept only one ID.&lt;/P&gt;&lt;P&gt;Thank you very much&lt;/P&gt;</description>
    <pubDate>Sat, 09 Jan 2021 06:02:40 GMT</pubDate>
    <dc:creator>2194133213</dc:creator>
    <dc:date>2021-01-09T06:02:40Z</dc:date>
    <item>
      <title>s32k144 flexCAN MB</title>
      <link>https://community.nxp.com/t5/S32K/s32k144-flexCAN-MB/m-p/1209189#M9536</link>
      <description>&lt;P&gt;I have a question.&lt;BR /&gt;How is the FLEXCAN_DRV_Receive function configured to receive multiple IDs?&lt;BR /&gt;The FLEXCAN_DRV_ConfigTxMb function is configured to accept only one ID.&lt;/P&gt;&lt;P&gt;Thank you very much&lt;/P&gt;</description>
      <pubDate>Sat, 09 Jan 2021 06:02:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k144-flexCAN-MB/m-p/1209189#M9536</guid>
      <dc:creator>2194133213</dc:creator>
      <dc:date>2021-01-09T06:02:40Z</dc:date>
    </item>
    <item>
      <title>Re: s32k144 flexCAN MB</title>
      <link>https://community.nxp.com/t5/S32K/s32k144-flexCAN-MB/m-p/1209387#M9539</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;Please refer: &lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/S32K1xx-SDK-FlexCAN-sample-projects-to-demonstrate-its-basic-and/ta-p/1172891" target="_self"&gt;S32K1xx SDK FlexCAN sample projects to demonstrate its basic and advanced features&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Mon, 11 Jan 2021 05:19:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k144-flexCAN-MB/m-p/1209387#M9539</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2021-01-11T05:19:13Z</dc:date>
    </item>
  </channel>
</rss>