<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32K188 runs with debugger, but not witout in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K188-runs-with-debugger-but-not-witout/m-p/1205342#M9430</link>
    <description>&lt;P&gt;Hi Robin.&lt;/P&gt;&lt;P&gt;I'm trying to solve same problem. but I can't see the tap that you let me see.&lt;/P&gt;&lt;P&gt;I think that's because I have another version S32DS.&lt;/P&gt;&lt;P&gt;I have&amp;nbsp;S32 Design Studio for S32 Platform&lt;BR /&gt;&amp;nbsp;- Version: 3.3&lt;BR /&gt;&amp;nbsp;- Build id: 200610&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="image.png" style="width: 503px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/133708i143292937FA5E0F6/image-size/large?v=v2&amp;amp;px=999" role="button" title="image.png" alt="image.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I want to execute S32K188 without debugger.&lt;/P&gt;&lt;P&gt;What can I do?&lt;/P&gt;</description>
    <pubDate>Thu, 31 Dec 2020 00:18:40 GMT</pubDate>
    <dc:creator>종찬박</dc:creator>
    <dc:date>2020-12-31T00:18:40Z</dc:date>
    <item>
      <title>S32K188 runs with debugger, but not witout</title>
      <link>https://community.nxp.com/t5/S32K/S32K188-runs-with-debugger-but-not-witout/m-p/1203150#M9360</link>
      <description>&lt;P&gt;Hi there,&lt;/P&gt;&lt;P&gt;I have created a project with "S32DS Application project" button, over the S32k188 micro controller; it just a blinking led. Works fine debugging with the Mutilink Universal debugger; BUT I unplug this debugger and after a reset the led is fix to OFF. Seems that the microcontroller doesn't start to run. I have set the optimization to "None".&lt;/P&gt;&lt;P&gt;I have tried a "S32DS Project from example" button (hello_world_s32k118) and adding the blinking led code; and works fine with and without debugger!!!!!!&lt;/P&gt;&lt;P&gt;There is something different inside the project parameters, between the example and the application. I have compared them and matched some parameters, but with the same results.&lt;/P&gt;&lt;P&gt;IDE:&amp;nbsp;&amp;nbsp; S32 Design Studio for ARM&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Version: 2.2&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Build id: 200116&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Where I could be failing?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;thanks a lot&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 22 Dec 2020 16:28:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K188-runs-with-debugger-but-not-witout/m-p/1203150#M9360</guid>
      <dc:creator>albertgalofre</dc:creator>
      <dc:date>2020-12-22T16:28:48Z</dc:date>
    </item>
    <item>
      <title>Re: S32K188 runs with debugger, but not witout</title>
      <link>https://community.nxp.com/t5/S32K/S32K188-runs-with-debugger-but-not-witout/m-p/1203837#M9373</link>
      <description>&lt;P&gt;Hi&amp;nbsp;albertgalofre,&lt;/P&gt;
&lt;P&gt;Please add "&lt;STRONG&gt;START_FROM_FLASH&lt;/STRONG&gt;" Symbols in "&lt;STRONG&gt;Standard S32DS Assembler&lt;/STRONG&gt;".&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="START_FROM_FLASH Standard S32DS Assembler Symbols.png" style="width: 670px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/133447iFE482BE10CF617F3/image-size/large?v=v2&amp;amp;px=999" role="button" title="START_FROM_FLASH Standard S32DS Assembler Symbols.png" alt="START_FROM_FLASH Standard S32DS Assembler Symbols.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Thu, 24 Dec 2020 00:57:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K188-runs-with-debugger-but-not-witout/m-p/1203837#M9373</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2020-12-24T00:57:32Z</dc:date>
    </item>
    <item>
      <title>Re: S32K188 runs with debugger, but not witout</title>
      <link>https://community.nxp.com/t5/S32K/S32K188-runs-with-debugger-but-not-witout/m-p/1204370#M9397</link>
      <description>&lt;P&gt;understood, done and running!!!!!&lt;/P&gt;&lt;P&gt;Bravo for you, and bravo for the NXPCommunity.&lt;/P&gt;&lt;P&gt;Thanks a lot&lt;/P&gt;</description>
      <pubDate>Sun, 27 Dec 2020 17:13:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K188-runs-with-debugger-but-not-witout/m-p/1204370#M9397</guid>
      <dc:creator>albertgalofre</dc:creator>
      <dc:date>2020-12-27T17:13:44Z</dc:date>
    </item>
    <item>
      <title>Re: S32K188 runs with debugger, but not witout</title>
      <link>https://community.nxp.com/t5/S32K/S32K188-runs-with-debugger-but-not-witout/m-p/1205342#M9430</link>
      <description>&lt;P&gt;Hi Robin.&lt;/P&gt;&lt;P&gt;I'm trying to solve same problem. but I can't see the tap that you let me see.&lt;/P&gt;&lt;P&gt;I think that's because I have another version S32DS.&lt;/P&gt;&lt;P&gt;I have&amp;nbsp;S32 Design Studio for S32 Platform&lt;BR /&gt;&amp;nbsp;- Version: 3.3&lt;BR /&gt;&amp;nbsp;- Build id: 200610&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="image.png" style="width: 503px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/133708i143292937FA5E0F6/image-size/large?v=v2&amp;amp;px=999" role="button" title="image.png" alt="image.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I want to execute S32K188 without debugger.&lt;/P&gt;&lt;P&gt;What can I do?&lt;/P&gt;</description>
      <pubDate>Thu, 31 Dec 2020 00:18:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K188-runs-with-debugger-but-not-witout/m-p/1205342#M9430</guid>
      <dc:creator>종찬박</dc:creator>
      <dc:date>2020-12-31T00:18:40Z</dc:date>
    </item>
    <item>
      <title>Re: S32K188 runs with debugger, but not witout</title>
      <link>https://community.nxp.com/t5/S32K/S32K188-runs-with-debugger-but-not-witout/m-p/1205346#M9431</link>
      <description>&lt;P&gt;Yes. There is a little different between S32DS 2.2 and 3.3.&lt;BR /&gt;You can open &lt;STRONG&gt;Standard S32DS Assembler&lt;/STRONG&gt; -&amp;gt; &lt;STRONG&gt;Preprocessor&lt;/STRONG&gt; and then add &lt;STRONG&gt;START_FROM_FLASH&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="START_FROM_FLASH S32 Design Studio for S32 Platform 3.3.png" style="width: 731px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/133709iC74FA34CA9AF0BEC/image-size/large?v=v2&amp;amp;px=999" role="button" title="START_FROM_FLASH S32 Design Studio for S32 Platform 3.3.png" alt="START_FROM_FLASH S32 Design Studio for S32 Platform 3.3.png" /&gt;&lt;/span&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 31 Dec 2020 00:33:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K188-runs-with-debugger-but-not-witout/m-p/1205346#M9431</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2020-12-31T00:33:19Z</dc:date>
    </item>
    <item>
      <title>Re: S32K188 runs with debugger, but not witout</title>
      <link>https://community.nxp.com/t5/S32K/S32K188-runs-with-debugger-but-not-witout/m-p/1205360#M9432</link>
      <description>&lt;P&gt;I'm afraid that it doesn't work.&lt;/P&gt;&lt;P&gt;I did already what you said so, but my board doesn't work.&lt;/P&gt;&lt;P&gt;when I control my board with debugger, it works well.&lt;/P&gt;&lt;P&gt;but, After power reset, it doesn't work.&lt;/P&gt;</description>
      <pubDate>Thu, 31 Dec 2020 02:54:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K188-runs-with-debugger-but-not-witout/m-p/1205360#M9432</guid>
      <dc:creator>종찬박</dc:creator>
      <dc:date>2020-12-31T02:54:25Z</dc:date>
    </item>
    <item>
      <title>Re: S32K188 runs with debugger, but not witout</title>
      <link>https://community.nxp.com/t5/S32K/S32K188-runs-with-debugger-but-not-witout/m-p/1860911#M35073</link>
      <description>&lt;P&gt;I followed your instructions, but it didn't work. I am using the routine of S32K312&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="binZhang01_0-1715130891904.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/277578iD8F044BD9FED92AE/image-size/medium?v=v2&amp;amp;px=400" role="button" title="binZhang01_0-1715130891904.png" alt="binZhang01_0-1715130891904.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="binZhang01_2-1715130935851.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/277580i45E84AD24AF76738/image-size/medium?v=v2&amp;amp;px=400" role="button" title="binZhang01_2-1715130935851.png" alt="binZhang01_2-1715130935851.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 08 May 2024 01:15:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K188-runs-with-debugger-but-not-witout/m-p/1860911#M35073</guid>
      <dc:creator>binZhang01</dc:creator>
      <dc:date>2024-05-08T01:15:18Z</dc:date>
    </item>
    <item>
      <title>Re: S32K188 runs with debugger, but not witout</title>
      <link>https://community.nxp.com/t5/S32K/S32K188-runs-with-debugger-but-not-witout/m-p/1884213#M36390</link>
      <description>It does not work when I try this method to debug S32K312 EVB.</description>
      <pubDate>Mon, 10 Jun 2024 12:03:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K188-runs-with-debugger-but-not-witout/m-p/1884213#M36390</guid>
      <dc:creator>Luxls</dc:creator>
      <dc:date>2024-06-10T12:03:19Z</dc:date>
    </item>
    <item>
      <title>Re: S32K188 runs with debugger, but not witout</title>
      <link>https://community.nxp.com/t5/S32K/S32K188-runs-with-debugger-but-not-witout/m-p/1884543#M36413</link>
      <description>&lt;P&gt;Please see the discussion here:&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32K/If-I-don-t-give-s32k312-delay-the-CAN-stop-during-operation/m-p/1828163/highlight/false#M32968" target="_self"&gt;If I don't give s32k312 delay, the CAN stop during operation&lt;/A&gt;&lt;BR /&gt;If the problem is still not solved, it is recommended to click ASK A QUESTION in the &lt;A href="https://community.nxp.com/t5/S32K/bd-p/S32K" target="_self"&gt;S32K community&lt;/A&gt;.&lt;/P&gt;</description>
      <pubDate>Tue, 11 Jun 2024 00:18:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K188-runs-with-debugger-but-not-witout/m-p/1884543#M36413</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2024-06-11T00:18:24Z</dc:date>
    </item>
  </channel>
</rss>