<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: Difference in receiving CAN messages using mailbox and using RxFiFO</title>
    <link>https://community.nxp.com/t5/S32K/Difference-in-receiving-CAN-messages-using-mailbox-and-using/m-p/1205285#M9428</link>
    <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/180999"&gt;@kishore_nxp&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;This will depend on the recurrence of the package. If in the system there's a package being processed in the module and a new transfer is not set, using the mailbox the package will be lost but this depends on the application and the data &lt;SPAN&gt;traffic&lt;/SPAN&gt;.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Alexis andalon&lt;/P&gt;</description>
    <pubDate>Wed, 30 Dec 2020 16:54:33 GMT</pubDate>
    <dc:creator>Alexis_A</dc:creator>
    <dc:date>2020-12-30T16:54:33Z</dc:date>
    <item>
      <title>Difference in receiving CAN messages using mailbox and using RxFiFO</title>
      <link>https://community.nxp.com/t5/S32K/Difference-in-receiving-CAN-messages-using-mailbox-and-using/m-p/1204282#M9393</link>
      <description>&lt;P&gt;Hello NXP Engineers,&lt;/P&gt;&lt;P&gt;What are difference between using Mailbox and RxFIFO in receiving CAN messages??&lt;/P&gt;&lt;P&gt;Are chances of losing CAN messages high on using Mailbox ??&lt;/P&gt;&lt;P&gt;plz help&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 25 Dec 2020 09:19:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Difference-in-receiving-CAN-messages-using-mailbox-and-using/m-p/1204282#M9393</guid>
      <dc:creator>kishore_nxp</dc:creator>
      <dc:date>2020-12-25T09:19:02Z</dc:date>
    </item>
    <item>
      <title>Re: Difference in receiving CAN messages using mailbox and using RxFiFO</title>
      <link>https://community.nxp.com/t5/S32K/Difference-in-receiving-CAN-messages-using-mailbox-and-using/m-p/1205285#M9428</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/180999"&gt;@kishore_nxp&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;This will depend on the recurrence of the package. If in the system there's a package being processed in the module and a new transfer is not set, using the mailbox the package will be lost but this depends on the application and the data &lt;SPAN&gt;traffic&lt;/SPAN&gt;.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Alexis andalon&lt;/P&gt;</description>
      <pubDate>Wed, 30 Dec 2020 16:54:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Difference-in-receiving-CAN-messages-using-mailbox-and-using/m-p/1205285#M9428</guid>
      <dc:creator>Alexis_A</dc:creator>
      <dc:date>2020-12-30T16:54:33Z</dc:date>
    </item>
  </channel>
</rss>