<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: How to unlock S32K148 Chip in S32K</title>
    <link>https://community.nxp.com/t5/S32K/How-to-unlock-S32K148-Chip/m-p/1204055#M9384</link>
    <description>&lt;P&gt;Hello Alexis,&lt;/P&gt;&lt;P&gt;I unlocked the ECU successfully!&lt;/P&gt;&lt;P&gt;The hints are: connect the Reset Pin (in JTAG) to the GND. Then, performing the unlocking procedure. After that, I loaded the correct source code (srec file) by Production Programming. Now the ECU is alive.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;</description>
    <pubDate>Thu, 24 Dec 2020 08:45:29 GMT</pubDate>
    <dc:creator>VinhNguyen13</dc:creator>
    <dc:date>2020-12-24T08:45:29Z</dc:date>
    <item>
      <title>How to unlock S32K148 Chip</title>
      <link>https://community.nxp.com/t5/S32K/How-to-unlock-S32K148-Chip/m-p/1201568#M9305</link>
      <description>&lt;P&gt;I used J-Link V9 to connect and flash SW for FS32K148 chip, but I faced this issue as picture below.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="VinhNguyen13_0-1608265265033.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/133025i92259E1802DD0FB9/image-size/medium?v=v2&amp;amp;px=400" role="button" title="VinhNguyen13_0-1608265265033.png" alt="VinhNguyen13_0-1608265265033.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;From my understanding, my chip is locked due to the wrong data is written to the flash at Address 0x400 -&amp;gt; 0x40F (related to protection bytes).&lt;/P&gt;&lt;P&gt;I tried to unlock chip by command:&lt;/P&gt;&lt;P&gt;[&lt;/P&gt;&lt;P&gt;J-Link&amp;gt;r0 // pull reset pin low&lt;/P&gt;&lt;P&gt;J-Link&amp;gt;swdwritedp 2,0x01000000 // MDM_AP status register&lt;/P&gt;&lt;P&gt;J-Link&amp;gt;swdreadap 0 // Read MDM_AP status register&lt;BR /&gt;J-Link&amp;gt;swdreadap 0 // Read MDM_AP status register (has to be done 2x) Flash memory ready and Mass erase enable bits should be set&lt;/P&gt;&lt;P&gt;J-Link&amp;gt;swdreadap 1 // Read MDM_AP control register&lt;BR /&gt;J-Link&amp;gt;swdreadap 1 // Read MDM_AP control register (has to be done 2x)&lt;/P&gt;&lt;P&gt;J-Link&amp;gt;unlock Kinetis // Erase and unsecure the MCU&lt;/P&gt;&lt;P&gt;]&lt;/P&gt;&lt;P&gt;But I can't. The error shown that:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="VinhNguyen13_1-1608265584055.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/133026i6FFFD8E115195DB7/image-size/medium?v=v2&amp;amp;px=400" role="button" title="VinhNguyen13_1-1608265584055.png" alt="VinhNguyen13_1-1608265584055.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="VinhNguyen13_2-1608265600338.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/133027i86D32EA894D9802B/image-size/medium?v=v2&amp;amp;px=400" role="button" title="VinhNguyen13_2-1608265600338.png" alt="VinhNguyen13_2-1608265600338.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there anyone faced this issue? Could you please to support for fixing this.&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 18 Dec 2020 04:27:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/How-to-unlock-S32K148-Chip/m-p/1201568#M9305</guid>
      <dc:creator>VinhNguyen13</dc:creator>
      <dc:date>2020-12-18T04:27:19Z</dc:date>
    </item>
    <item>
      <title>Re: How to unlock S32K148 Chip</title>
      <link>https://community.nxp.com/t5/S32K/How-to-unlock-S32K148-Chip/m-p/1203916#M9379</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/178685"&gt;@VinhNguyen13&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Writing to this register without taking care of the bits written will lock the MCU without the recovery option and for the messages in the debug probe looks like that this is the case.&amp;nbsp; You can take a look at the description of this register at the RM&amp;nbsp;36.4.1 Flash configuration field description.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Alexis Andalon&lt;/P&gt;</description>
      <pubDate>Thu, 24 Dec 2020 03:34:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/How-to-unlock-S32K148-Chip/m-p/1203916#M9379</guid>
      <dc:creator>Alexis_A</dc:creator>
      <dc:date>2020-12-24T03:34:18Z</dc:date>
    </item>
    <item>
      <title>Re: How to unlock S32K148 Chip</title>
      <link>https://community.nxp.com/t5/S32K/How-to-unlock-S32K148-Chip/m-p/1204055#M9384</link>
      <description>&lt;P&gt;Hello Alexis,&lt;/P&gt;&lt;P&gt;I unlocked the ECU successfully!&lt;/P&gt;&lt;P&gt;The hints are: connect the Reset Pin (in JTAG) to the GND. Then, performing the unlocking procedure. After that, I loaded the correct source code (srec file) by Production Programming. Now the ECU is alive.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;</description>
      <pubDate>Thu, 24 Dec 2020 08:45:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/How-to-unlock-S32K148-Chip/m-p/1204055#M9384</guid>
      <dc:creator>VinhNguyen13</dc:creator>
      <dc:date>2020-12-24T08:45:29Z</dc:date>
    </item>
    <item>
      <title>Re: How to unlock S32K148 Chip</title>
      <link>https://community.nxp.com/t5/S32K/How-to-unlock-S32K148-Chip/m-p/1327795#M11770</link>
      <description>&lt;P&gt;&lt;A href="https://community.nxp.com/t5/user/viewprofilepage/user-id/178685" target="_self"&gt;&lt;SPAN class=""&gt;Hi &lt;/SPAN&gt;&lt;/A&gt;&lt;A href="https://community.nxp.com/t5/user/viewprofilepage/user-id/178685" target="_self"&gt;&lt;SPAN class=""&gt;VinhNguyen13&lt;/SPAN&gt;&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;I am also facing the same issue. Getting time out error while unlocking the device. I have followed the procedure as mentioned. I have connected reset pin to ground and executed the J-Link commands as follows&lt;/P&gt;&lt;P&gt;J-Link&amp;gt;r0&lt;/P&gt;&lt;P&gt;J-Link&amp;gt;si 1&lt;/P&gt;&lt;P&gt;J-Link&amp;gt;swdselect&lt;/P&gt;&lt;P&gt;J-Link&amp;gt;swdwritedp 2, 0x01000000&lt;/P&gt;&lt;P&gt;J-Link&amp;gt;swdreadap 0&lt;/P&gt;&lt;P&gt;J-Link&amp;gt;swdreadap 0&lt;/P&gt;&lt;P&gt;J-Link&amp;gt;swdreadap 1&lt;/P&gt;&lt;P&gt;J-Link&amp;gt;swdreadap 1&lt;/P&gt;&lt;P&gt;J-Link&amp;gt;unlock Kinetis&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="J-Link Command line Unlock.png" style="width: 418px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/153727i153508EC40F518F0/image-size/large?v=v2&amp;amp;px=999" role="button" title="J-Link Command line Unlock.png" alt="J-Link Command line Unlock.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Am I missing anything here? Thanks&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 23 Aug 2021 12:40:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/How-to-unlock-S32K148-Chip/m-p/1327795#M11770</guid>
      <dc:creator>KiranE</dc:creator>
      <dc:date>2021-08-23T12:40:07Z</dc:date>
    </item>
  </channel>
</rss>