<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックCould sector will be divided into blocks?</title>
    <link>https://community.nxp.com/t5/S32K/Could-sector-will-be-divided-into-blocks/m-p/1203917#M9380</link>
    <description>&lt;P&gt;Hello&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; I&amp;nbsp; see datasheet S32K-RM, find that the program flash memory and data flash memory just have divided into sectors. Because I use the MCU S2K116(P-Flash 128KB, D-Flash 32KB). the size of sector for the&amp;nbsp;&amp;nbsp;P-Flash and D-Flash are 2KB.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;&amp;nbsp;Are there any smaller units under the sector? for example blocks? If I want to operate the D-Flash,&amp;nbsp;The smallest unit of operation is a sector?&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 24 Dec 2020 03:36:42 GMT</pubDate>
    <dc:creator>asd046012</dc:creator>
    <dc:date>2020-12-24T03:36:42Z</dc:date>
    <item>
      <title>Could sector will be divided into blocks?</title>
      <link>https://community.nxp.com/t5/S32K/Could-sector-will-be-divided-into-blocks/m-p/1203917#M9380</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; I&amp;nbsp; see datasheet S32K-RM, find that the program flash memory and data flash memory just have divided into sectors. Because I use the MCU S2K116(P-Flash 128KB, D-Flash 32KB). the size of sector for the&amp;nbsp;&amp;nbsp;P-Flash and D-Flash are 2KB.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;&amp;nbsp;Are there any smaller units under the sector? for example blocks? If I want to operate the D-Flash,&amp;nbsp;The smallest unit of operation is a sector?&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 24 Dec 2020 03:36:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Could-sector-will-be-divided-into-blocks/m-p/1203917#M9380</guid>
      <dc:creator>asd046012</dc:creator>
      <dc:date>2020-12-24T03:36:42Z</dc:date>
    </item>
    <item>
      <title>Re: Could sector will be divided into blocks?</title>
      <link>https://community.nxp.com/t5/S32K/Could-sector-will-be-divided-into-blocks/m-p/1205059#M9417</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/165390"&gt;@asd046012&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Do you try to manage the memory in smaller sections in run time? In this case, there's a command called&amp;nbsp;Program Phrase that allows to program 8 bytes. For more information, check section&amp;nbsp;36.5.9.2 Flash commands in the RM.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Alexis Andalon&lt;/P&gt;</description>
      <pubDate>Wed, 30 Dec 2020 00:07:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Could-sector-will-be-divided-into-blocks/m-p/1205059#M9417</guid>
      <dc:creator>Alexis_A</dc:creator>
      <dc:date>2020-12-30T00:07:37Z</dc:date>
    </item>
  </channel>
</rss>