<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32K144 VCC short to GND after power on in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K144-VCC-short-to-GND-after-power-on/m-p/1202018#M9323</link>
    <description>&lt;P&gt;Hi Robin,&lt;/P&gt;&lt;P&gt;Thank you for your suggestion.&lt;/P&gt;&lt;P&gt;I have made a new pcb and solely solder the power supply pins of the mcu. I have also put a zener diode at the output of the LDO. It works. There is no short circuit any more. The circuit draws about 20mA with no software flashed.&lt;/P&gt;&lt;P&gt;I will try to program the mcu at the next step.&lt;/P&gt;</description>
    <pubDate>Sun, 20 Dec 2020 13:48:57 GMT</pubDate>
    <dc:creator>Jimny</dc:creator>
    <dc:date>2020-12-20T13:48:57Z</dc:date>
    <item>
      <title>S32K144 VCC short to GND after power on</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-VCC-short-to-GND-after-power-on/m-p/1198388#M9221</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I designed a minimum system with S32K144, please see the schematic in the attachment. And then I made a pcb and solder the components.&lt;/P&gt;&lt;P&gt;When I power on the board with a DC power source which outputs a 7V voltage to the LDO on the board, an short circuit occured. After some measurement with multi-meter, I found VCC is short to GND. So I take the MCU off the board and there is no short circuit.&lt;/P&gt;&lt;P&gt;It is obvious that the MCU is internally short-circuited. What's wrong with the schematic? How to get rid of the problem? Can anyone help?&lt;/P&gt;</description>
      <pubDate>Sun, 13 Dec 2020 12:25:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-VCC-short-to-GND-after-power-on/m-p/1198388#M9221</guid>
      <dc:creator>Jimny</dc:creator>
      <dc:date>2020-12-13T12:25:21Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 VCC short to GND after power on</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-VCC-short-to-GND-after-power-on/m-p/1198477#M9227</link>
      <description>&lt;P&gt;Hi&amp;nbsp;ZZD,&lt;/P&gt;
&lt;P&gt;I did not find out error in your schematic.&lt;BR /&gt;Please check the PCB file and measure the pads on board. &lt;BR /&gt;For example:&lt;BR /&gt;pin 7\8\9\41 connect to 5VDC&lt;BR /&gt;pin 10\40 connect to GND&lt;/P&gt;
&lt;P&gt;If you doubt that the MCU is internally short-circuited, you can measure pads of MCU before solder it on PCB board.&lt;/P&gt;
&lt;P&gt;Please check if the MCU is place correctly with PCB pads.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Pin1.jpg" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/132523i7AEF38D5E4D8452E/image-size/large?v=v2&amp;amp;px=999" role="button" title="Pin1.jpg" alt="Pin1.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;I am not quite sure if this MCU has exposed pad (EP) at bottom. If so:&lt;BR /&gt;The bottom of the package provides the primary heat removal path, as well as excellent electrical grounding to the PCB through an exposed pad (EP).&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Mon, 14 Dec 2020 02:58:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-VCC-short-to-GND-after-power-on/m-p/1198477#M9227</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2020-12-14T02:58:16Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 VCC short to GND after power on</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-VCC-short-to-GND-after-power-on/m-p/1202018#M9323</link>
      <description>&lt;P&gt;Hi Robin,&lt;/P&gt;&lt;P&gt;Thank you for your suggestion.&lt;/P&gt;&lt;P&gt;I have made a new pcb and solely solder the power supply pins of the mcu. I have also put a zener diode at the output of the LDO. It works. There is no short circuit any more. The circuit draws about 20mA with no software flashed.&lt;/P&gt;&lt;P&gt;I will try to program the mcu at the next step.&lt;/P&gt;</description>
      <pubDate>Sun, 20 Dec 2020 13:48:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-VCC-short-to-GND-after-power-on/m-p/1202018#M9323</guid>
      <dc:creator>Jimny</dc:creator>
      <dc:date>2020-12-20T13:48:57Z</dc:date>
    </item>
  </channel>
</rss>