<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32Kのトピックsd card activate using interrupt</title>
    <link>https://community.nxp.com/t5/S32K/sd-card-activate-using-interrupt/m-p/1201715#M9311</link>
    <description>&lt;P&gt;Hi there,&lt;/P&gt;&lt;P&gt;I'am using SPI protocol for SD card communication , now i have to implement protocol using interrupt mean when slave detect then only spi should works because iam using bare metal programming , when sd card absent that should not have to stop the remaining tasks.&lt;/P&gt;&lt;P&gt;Thanks in advance ..&lt;/P&gt;</description>
    <pubDate>Fri, 18 Dec 2020 09:02:50 GMT</pubDate>
    <dc:creator>Teja114</dc:creator>
    <dc:date>2020-12-18T09:02:50Z</dc:date>
    <item>
      <title>sd card activate using interrupt</title>
      <link>https://community.nxp.com/t5/S32K/sd-card-activate-using-interrupt/m-p/1201715#M9311</link>
      <description>&lt;P&gt;Hi there,&lt;/P&gt;&lt;P&gt;I'am using SPI protocol for SD card communication , now i have to implement protocol using interrupt mean when slave detect then only spi should works because iam using bare metal programming , when sd card absent that should not have to stop the remaining tasks.&lt;/P&gt;&lt;P&gt;Thanks in advance ..&lt;/P&gt;</description>
      <pubDate>Fri, 18 Dec 2020 09:02:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/sd-card-activate-using-interrupt/m-p/1201715#M9311</guid>
      <dc:creator>Teja114</dc:creator>
      <dc:date>2020-12-18T09:02:50Z</dc:date>
    </item>
    <item>
      <title>Re: sd card activate using interrupt</title>
      <link>https://community.nxp.com/t5/S32K/sd-card-activate-using-interrupt/m-p/1204533#M9401</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I'm afraid this is too application-dependent.&lt;/P&gt;
&lt;P&gt;And the description is not very clear.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR, Daniel&lt;/P&gt;</description>
      <pubDate>Mon, 28 Dec 2020 10:32:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/sd-card-activate-using-interrupt/m-p/1204533#M9401</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2020-12-28T10:32:18Z</dc:date>
    </item>
    <item>
      <title>Re: sd card activate using interrupt</title>
      <link>https://community.nxp.com/t5/S32K/sd-card-activate-using-interrupt/m-p/1204536#M9402</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/160001"&gt;@danielmartynek&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;I want to write LPSPI code with interrupt method for S32k142 device .&lt;/P&gt;&lt;P&gt;currently iam using polling method.&lt;/P&gt;&lt;P&gt;can you please guide us how to write LPSPI driver using interrupt method&lt;/P&gt;</description>
      <pubDate>Mon, 28 Dec 2020 11:00:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/sd-card-activate-using-interrupt/m-p/1204536#M9402</guid>
      <dc:creator>Teja114</dc:creator>
      <dc:date>2020-12-28T11:00:05Z</dc:date>
    </item>
    <item>
      <title>Re: sd card activate using interrupt</title>
      <link>https://community.nxp.com/t5/S32K/sd-card-activate-using-interrupt/m-p/1205605#M9442</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Please refer to the SDK LPSPI driver.&lt;/P&gt;
&lt;P&gt;You can start with the lpspi_transfer_s32k142 SDK example that you can find in the S32 Design Studio.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;</description>
      <pubDate>Sat, 02 Jan 2021 16:31:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/sd-card-activate-using-interrupt/m-p/1205605#M9442</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2021-01-02T16:31:54Z</dc:date>
    </item>
  </channel>
</rss>