<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 MCSXTE2BK142 Development Board - Motor Speed Control</title>
    <link>https://community.nxp.com/t5/S32K/MCSXTE2BK142-Development-Board-Motor-Speed-Control/m-p/1201432#M9300</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have recently purchased the MCSXTE2BK142 development board for evaluation of the S32K142 MCU. Per document&amp;nbsp;MCSXTE2BK142HWUG section 3.5, the motor speed and direction can be set by LIN, CAN or PWM communication, or via a potentiometer (designated as R73) connected to an ADC input on the MCU.&lt;/P&gt;&lt;P&gt;I have downloaded the software provided for this board (MCSXTE2BK142_SW), but from my review of the software I am unable to see where speed control using the potentiometer is incorporated into the software. From reviewing the schematic for this board, I can see that the Analog Input signal is connected to ADC0 CH14, however I cannot find this channel being read anywhere in the software.&lt;/P&gt;&lt;P&gt;I'm hoping to see if anyone familiar with this board has experience using the potentiometer for speed control, and can point out to me if/how it is incorporated in the software.&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Peyton&lt;/P&gt;</description>
    <pubDate>Thu, 17 Dec 2020 23:41:55 GMT</pubDate>
    <dc:creator>peytonu5</dc:creator>
    <dc:date>2020-12-17T23:41:55Z</dc:date>
    <item>
      <title>MCSXTE2BK142 Development Board - Motor Speed Control</title>
      <link>https://community.nxp.com/t5/S32K/MCSXTE2BK142-Development-Board-Motor-Speed-Control/m-p/1201432#M9300</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have recently purchased the MCSXTE2BK142 development board for evaluation of the S32K142 MCU. Per document&amp;nbsp;MCSXTE2BK142HWUG section 3.5, the motor speed and direction can be set by LIN, CAN or PWM communication, or via a potentiometer (designated as R73) connected to an ADC input on the MCU.&lt;/P&gt;&lt;P&gt;I have downloaded the software provided for this board (MCSXTE2BK142_SW), but from my review of the software I am unable to see where speed control using the potentiometer is incorporated into the software. From reviewing the schematic for this board, I can see that the Analog Input signal is connected to ADC0 CH14, however I cannot find this channel being read anywhere in the software.&lt;/P&gt;&lt;P&gt;I'm hoping to see if anyone familiar with this board has experience using the potentiometer for speed control, and can point out to me if/how it is incorporated in the software.&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Peyton&lt;/P&gt;</description>
      <pubDate>Thu, 17 Dec 2020 23:41:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/MCSXTE2BK142-Development-Board-Motor-Speed-Control/m-p/1201432#M9300</guid>
      <dc:creator>peytonu5</dc:creator>
      <dc:date>2020-12-17T23:41:55Z</dc:date>
    </item>
    <item>
      <title>Re: MCSXTE2BK142 Development Board - Motor Speed Control</title>
      <link>https://community.nxp.com/t5/S32K/MCSXTE2BK142-Development-Board-Motor-Speed-Control/m-p/1201816#M9316</link>
      <description>&lt;P&gt;Hello Peyton,&lt;/P&gt;
&lt;P&gt;The AN input is not a classic use case for automotive application, that is the reason we did not implement it.&lt;/P&gt;
&lt;P&gt;I have sent you a version of the SW that uses the analog signal to control the application.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;</description>
      <pubDate>Fri, 18 Dec 2020 12:47:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/MCSXTE2BK142-Development-Board-Motor-Speed-Control/m-p/1201816#M9316</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2020-12-18T12:47:31Z</dc:date>
    </item>
    <item>
      <title>Re: MCSXTE2BK142 Development Board - Motor Speed Control</title>
      <link>https://community.nxp.com/t5/S32K/MCSXTE2BK142-Development-Board-Motor-Speed-Control/m-p/1446149#M15034</link>
      <description>&lt;P&gt;Dear Mr. Daniel,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can you pls send me the code to control the BLDC motor with Analog input pin on the board via potentiometer R73.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;X Ignatius&lt;/P&gt;</description>
      <pubDate>Wed, 20 Apr 2022 06:45:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/MCSXTE2BK142-Development-Board-Motor-Speed-Control/m-p/1446149#M15034</guid>
      <dc:creator>Ignatius</dc:creator>
      <dc:date>2022-04-20T06:45:56Z</dc:date>
    </item>
    <item>
      <title>Re: MCSXTE2BK142 Development Board - Motor Speed Control</title>
      <link>https://community.nxp.com/t5/S32K/MCSXTE2BK142-Development-Board-Motor-Speed-Control/m-p/1446353#M15049</link>
      <description>&lt;P&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/199440"&gt;@Ignatius&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Please create a ticket?&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="danielmartynek_0-1650451150032.png" style="width: 573px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/177472iE6D17314F311632D/image-dimensions/573x301?v=v2" width="573" height="301" role="button" title="danielmartynek_0-1650451150032.png" alt="danielmartynek_0-1650451150032.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Thank you,&lt;/P&gt;
&lt;P&gt;BR, Daniel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 20 Apr 2022 10:39:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/MCSXTE2BK142-Development-Board-Motor-Speed-Control/m-p/1446353#M15049</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2022-04-20T10:39:54Z</dc:date>
    </item>
    <item>
      <title>Re: MCSXTE2BK142 Development Board - Motor Speed Control</title>
      <link>https://community.nxp.com/t5/S32K/MCSXTE2BK142-Development-Board-Motor-Speed-Control/m-p/1447170#M15063</link>
      <description>&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;P&gt;Dear Daniel,&lt;/P&gt;&lt;P&gt;Created the ticket.&lt;/P&gt;&lt;P&gt;Case Number :&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;00461818&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&lt;U&gt;Case Description&lt;/U&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;Subject : MCSXTE2BK142 Development Board - Motor Speed Control Description : Speed control of BLDC motor with the on board potentiometer R73. I need a sample code to run on MCSXTE2BK142&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;X Ignatius&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;</description>
      <pubDate>Thu, 21 Apr 2022 10:24:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/MCSXTE2BK142-Development-Board-Motor-Speed-Control/m-p/1447170#M15063</guid>
      <dc:creator>Ignatius</dc:creator>
      <dc:date>2022-04-21T10:24:23Z</dc:date>
    </item>
  </channel>
</rss>