<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックSCST in S32K146</title>
    <link>https://community.nxp.com/t5/S32K/SCST-in-S32K146/m-p/1201232#M9296</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;We are trying to integrate the SCST lib in our project which run on the S32K146 controller and the compiler used was GHS v2016.5.4.&lt;/P&gt;&lt;P&gt;After including the "-preprocess_assembly_files" in the cmake file, still we are getting the error as "The file "m4_scst_configuration.h" cannot open, error #......"&lt;/P&gt;&lt;P&gt;As per the manual "M4_S32K144_SCST_User_Manual", this SCST lib shall support the GHS compiler v2017.1.4 and v2017.5.4.&lt;/P&gt;&lt;P&gt;From the above statement, its is not possible to include other than those version in GHS? i.e. Not possible with the compiler v2016.5.4?&lt;/P&gt;</description>
    <pubDate>Thu, 17 Dec 2020 12:52:02 GMT</pubDate>
    <dc:creator>vishnukumar_n</dc:creator>
    <dc:date>2020-12-17T12:52:02Z</dc:date>
    <item>
      <title>SCST in S32K146</title>
      <link>https://community.nxp.com/t5/S32K/SCST-in-S32K146/m-p/1201232#M9296</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;We are trying to integrate the SCST lib in our project which run on the S32K146 controller and the compiler used was GHS v2016.5.4.&lt;/P&gt;&lt;P&gt;After including the "-preprocess_assembly_files" in the cmake file, still we are getting the error as "The file "m4_scst_configuration.h" cannot open, error #......"&lt;/P&gt;&lt;P&gt;As per the manual "M4_S32K144_SCST_User_Manual", this SCST lib shall support the GHS compiler v2017.1.4 and v2017.5.4.&lt;/P&gt;&lt;P&gt;From the above statement, its is not possible to include other than those version in GHS? i.e. Not possible with the compiler v2016.5.4?&lt;/P&gt;</description>
      <pubDate>Thu, 17 Dec 2020 12:52:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/SCST-in-S32K146/m-p/1201232#M9296</guid>
      <dc:creator>vishnukumar_n</dc:creator>
      <dc:date>2020-12-17T12:52:02Z</dc:date>
    </item>
    <item>
      <title>Re: SCST in S32K146</title>
      <link>https://community.nxp.com/t5/S32K/SCST-in-S32K146/m-p/1202529#M9342</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;when the header file cannot be open this is usually caused by not adding -I assembler option to tell assembler where the include files shall be searched for. For example in my project I have to add the following assembler option:&lt;/P&gt;
&lt;LI-CODE lang="markup"&gt;-I./SCST/src/h&lt;/LI-CODE&gt;
&lt;P&gt;It is needed to update the path after -I option to point to the folder where the&amp;nbsp;&amp;nbsp;&lt;SPAN&gt;m4_scst_configuration.h is located (in my case the path is ./SCST/src/h).&lt;BR /&gt;Regarding the compiler version, usually the SCST will work also with other versions of compiler but this was not checked nor tested. The only version which was tested is written in the SCST user manual (GHS compiler v2017.1.4 and v2017.5.4).&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Frantisek&lt;/P&gt;</description>
      <pubDate>Mon, 21 Dec 2020 14:28:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/SCST-in-S32K146/m-p/1202529#M9342</guid>
      <dc:creator>frantisekdobes</dc:creator>
      <dc:date>2020-12-21T14:28:59Z</dc:date>
    </item>
    <item>
      <title>Re: SCST in S32K146</title>
      <link>https://community.nxp.com/t5/S32K/SCST-in-S32K146/m-p/1203622#M9370</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/5071"&gt;@frantisekdobes&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;Thanks for your support, with the option -I we build the lib without any issue.&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Vishnu&lt;/P&gt;</description>
      <pubDate>Wed, 23 Dec 2020 09:55:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/SCST-in-S32K146/m-p/1203622#M9370</guid>
      <dc:creator>vishnukumar_n</dc:creator>
      <dc:date>2020-12-23T09:55:42Z</dc:date>
    </item>
  </channel>
</rss>