<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 Re: BLDC with s32k144</title>
    <link>https://community.nxp.com/t5/S32K/BLDC-with-s32k144/m-p/1201084#M9291</link>
    <description>&lt;P&gt;Hi Petervlna,&lt;/P&gt;&lt;P&gt;thank you for your answer. I changed it in the code (macro) of course. But my question was, if i can change it in Freemaster, for example like the Switch between on and off. Thank you for your help.&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Abdel&lt;/P&gt;</description>
    <pubDate>Thu, 17 Dec 2020 08:28:33 GMT</pubDate>
    <dc:creator>Abdel</dc:creator>
    <dc:date>2020-12-17T08:28:33Z</dc:date>
    <item>
      <title>BLDC with s32k144</title>
      <link>https://community.nxp.com/t5/S32K/BLDC-with-s32k144/m-p/1200567#M9281</link>
      <description>&lt;P&gt;Hi, can you help me to change rotation directory in Freemaster. I can only read a paramter rotationDir 0 (clockwise) or 1 (counterclockwise) but i can't control it. Or is there another parameter for it? Thank you in advance.&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Abdel&lt;/P&gt;</description>
      <pubDate>Wed, 16 Dec 2020 18:04:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/BLDC-with-s32k144/m-p/1200567#M9281</guid>
      <dc:creator>Abdel</dc:creator>
      <dc:date>2020-12-16T18:04:53Z</dc:date>
    </item>
    <item>
      <title>Re: BLDC with s32k144</title>
      <link>https://community.nxp.com/t5/S32K/BLDC-with-s32k144/m-p/1201060#M9289</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;For BLDC there is only one rotation direction implemented in MCAT.&lt;/P&gt;
&lt;P&gt;From freemaster of MCAT it is not possible to change direction.&lt;/P&gt;
&lt;P&gt;If you like to change dirrection you have to change the macro (rotationDir) in to source code, compile it and load application to micro.&lt;/P&gt;
&lt;P&gt;best regards,&lt;/P&gt;
&lt;P&gt;Peter&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 17 Dec 2020 08:02:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/BLDC-with-s32k144/m-p/1201060#M9289</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2020-12-17T08:02:19Z</dc:date>
    </item>
    <item>
      <title>Re: BLDC with s32k144</title>
      <link>https://community.nxp.com/t5/S32K/BLDC-with-s32k144/m-p/1201084#M9291</link>
      <description>&lt;P&gt;Hi Petervlna,&lt;/P&gt;&lt;P&gt;thank you for your answer. I changed it in the code (macro) of course. But my question was, if i can change it in Freemaster, for example like the Switch between on and off. Thank you for your help.&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Abdel&lt;/P&gt;</description>
      <pubDate>Thu, 17 Dec 2020 08:28:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/BLDC-with-s32k144/m-p/1201084#M9291</guid>
      <dc:creator>Abdel</dc:creator>
      <dc:date>2020-12-17T08:28:33Z</dc:date>
    </item>
    <item>
      <title>Re: BLDC with s32k144</title>
      <link>https://community.nxp.com/t5/S32K/BLDC-with-s32k144/m-p/1204291#M9394</link>
      <description>&lt;P&gt;Hi Petervlna,&lt;/P&gt;&lt;P&gt;I hope you had a niceevening. The variable is determined to be read from a file, it is stored somewhere logically I can change the variable in a file from freemaster before I start the program. Is that correct?&lt;/P&gt;&lt;P&gt;Thank you in advance&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Abdel&lt;/P&gt;</description>
      <pubDate>Fri, 25 Dec 2020 10:24:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/BLDC-with-s32k144/m-p/1204291#M9394</guid>
      <dc:creator>Abdel</dc:creator>
      <dc:date>2020-12-25T10:24:44Z</dc:date>
    </item>
  </channel>
</rss>