<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic FTM up counting configuration in S32K</title>
    <link>https://community.nxp.com/t5/S32K/FTM-up-counting-configuration/m-p/1199734#M9262</link>
    <description>&lt;P&gt;I am trying to use FTM as a up-counting timer simply, but CNT register value remains 0.&lt;/P&gt;&lt;P&gt;My settings are follows:&lt;BR /&gt;&lt;SPAN&gt;MOD = 0x2000&lt;BR /&gt;&lt;/SPAN&gt;CONF= 0xC0&lt;/P&gt;&lt;P&gt;Other registers are reset default values.&lt;BR /&gt;Finally, set 0x118 in the SC register.&lt;/P&gt;&lt;P&gt;I expected the CNT register to count up to 0x2000, but it remains 0.&lt;BR /&gt;The SC register shows 0x198 and the TOF remains 0, so I think the countup has not started.&lt;/P&gt;&lt;P&gt;The count clock is SIRCDIV1.&lt;/P&gt;&lt;P&gt;Are there any restrictions when using FTM as an up counting timer?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 15 Dec 2020 15:06:47 GMT</pubDate>
    <dc:creator>Hozumi</dc:creator>
    <dc:date>2020-12-15T15:06:47Z</dc:date>
    <item>
      <title>FTM up counting configuration</title>
      <link>https://community.nxp.com/t5/S32K/FTM-up-counting-configuration/m-p/1199734#M9262</link>
      <description>&lt;P&gt;I am trying to use FTM as a up-counting timer simply, but CNT register value remains 0.&lt;/P&gt;&lt;P&gt;My settings are follows:&lt;BR /&gt;&lt;SPAN&gt;MOD = 0x2000&lt;BR /&gt;&lt;/SPAN&gt;CONF= 0xC0&lt;/P&gt;&lt;P&gt;Other registers are reset default values.&lt;BR /&gt;Finally, set 0x118 in the SC register.&lt;/P&gt;&lt;P&gt;I expected the CNT register to count up to 0x2000, but it remains 0.&lt;BR /&gt;The SC register shows 0x198 and the TOF remains 0, so I think the countup has not started.&lt;/P&gt;&lt;P&gt;The count clock is SIRCDIV1.&lt;/P&gt;&lt;P&gt;Are there any restrictions when using FTM as an up counting timer?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 15 Dec 2020 15:06:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/FTM-up-counting-configuration/m-p/1199734#M9262</guid>
      <dc:creator>Hozumi</dc:creator>
      <dc:date>2020-12-15T15:06:47Z</dc:date>
    </item>
    <item>
      <title>Re: FTM up counting configuration</title>
      <link>https://community.nxp.com/t5/S32K/FTM-up-counting-configuration/m-p/1200058#M9267</link>
      <description>&lt;P&gt;Hi&amp;nbsp;Ken3,&lt;/P&gt;
&lt;P&gt;Please refer "&lt;EM&gt;Table 27-9. Peripheral module clocking (continued)&lt;/EM&gt;".&lt;BR /&gt;If you want to select &lt;STRONG&gt;SIRCDIV1_CLK&lt;/STRONG&gt; as counter clock, then &lt;STRONG&gt;External clock&lt;/STRONG&gt; should be select by &lt;STRONG&gt;FTMn_SC[CLKS]&lt;/STRONG&gt;.&lt;BR /&gt;But you select &lt;STRONG&gt;Fixed frequency clock&lt;/STRONG&gt; by &lt;STRONG&gt;FTMn_SC[CLKS]&lt;/STRONG&gt;.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Table 27-9. Peripheral module clocking (continued).png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/132771i578A048CF6AAE5A1/image-size/large?v=v2&amp;amp;px=999" role="button" title="Table 27-9. Peripheral module clocking (continued).png" alt="Table 27-9. Peripheral module clocking (continued).png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Wed, 16 Dec 2020 04:26:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/FTM-up-counting-configuration/m-p/1200058#M9267</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2020-12-16T04:26:34Z</dc:date>
    </item>
  </channel>
</rss>