<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: How to disable FlexCAN auto re-transmitting feature in S32K</title>
    <link>https://community.nxp.com/t5/S32K/How-to-disable-FlexCAN-auto-re-transmitting-feature/m-p/1195346#M9162</link>
    <description>&lt;P&gt;Hi Yuhui,&lt;/P&gt;
&lt;P&gt;there's no such option, this behavior is given by CAN spec.&lt;/P&gt;
&lt;P&gt;Solution is to connect another node which will acknowledge the message.&lt;/P&gt;
&lt;P&gt;Or, if it is for test purposes only, you can use internal loop back mode (LPB bit in CTRL1 register). In this mode, you will receive what you sent and ACK is ignored.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 08 Dec 2020 08:59:07 GMT</pubDate>
    <dc:creator>lukaszadrapa</dc:creator>
    <dc:date>2020-12-08T08:59:07Z</dc:date>
    <item>
      <title>How to disable FlexCAN auto re-transmitting feature</title>
      <link>https://community.nxp.com/t5/S32K/How-to-disable-FlexCAN-auto-re-transmitting-feature/m-p/1195092#M9159</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;My goal is to let FlexCAN always only send single-shot CAN message.&lt;/P&gt;
&lt;P&gt;I am currently using S32K144 SDK to play with FlexCAN.&lt;/P&gt;
&lt;P&gt;The current situation is, when a CAN message was not acknowledged by any receiver or any error was reported, the FlexCAN will repeatedly re-transmit this CAN message until it's ACKed or timeout.&lt;/P&gt;
&lt;P&gt;For some CAN messages, I just want FlexCAN to send message frame only once without any re-transmitting. Where is that magic reg/bits?&lt;/P&gt;
&lt;P&gt;Plus, much appreciate if you could provide an example code on that. (I am just new to S32K)&lt;/P&gt;
&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Tue, 08 Dec 2020 03:22:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/How-to-disable-FlexCAN-auto-re-transmitting-feature/m-p/1195092#M9159</guid>
      <dc:creator>YuhuiMa</dc:creator>
      <dc:date>2020-12-08T03:22:38Z</dc:date>
    </item>
    <item>
      <title>Re: How to disable FlexCAN auto re-transmitting feature</title>
      <link>https://community.nxp.com/t5/S32K/How-to-disable-FlexCAN-auto-re-transmitting-feature/m-p/1195346#M9162</link>
      <description>&lt;P&gt;Hi Yuhui,&lt;/P&gt;
&lt;P&gt;there's no such option, this behavior is given by CAN spec.&lt;/P&gt;
&lt;P&gt;Solution is to connect another node which will acknowledge the message.&lt;/P&gt;
&lt;P&gt;Or, if it is for test purposes only, you can use internal loop back mode (LPB bit in CTRL1 register). In this mode, you will receive what you sent and ACK is ignored.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 08 Dec 2020 08:59:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/How-to-disable-FlexCAN-auto-re-transmitting-feature/m-p/1195346#M9162</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2020-12-08T08:59:07Z</dc:date>
    </item>
  </channel>
</rss>