<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic pcssck in S32K</title>
    <link>https://community.nxp.com/t5/S32K/pcssck/m-p/1194268#M9139</link>
    <description>&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Target is S32K148.&lt;/P&gt;&lt;P&gt;I'm trying to do an SPI transfer consisting of 5 bytes(40 bits) where the CS is asserted for the duration of transfer. The baud rate is &amp;nbsp;4mhz, peripheral Clock is PLL and Divider is 1 and peripheral Clock frequency is 40mhz , using SPI0 for this I have the following in LPSPI0_CCR:&lt;/P&gt;&lt;P&gt;SCKDIV 0X08&lt;/P&gt;&lt;P&gt;DBT 0X04&lt;/P&gt;&lt;P&gt;PCSSCK 0X03&lt;/P&gt;&lt;P&gt;SCKPCS 0X03&lt;/P&gt;&lt;P&gt;Using these values results in an uneven clock and longer CS assertion period. when I twig these parameters the clock changes but I am not able to achieve the desired symmetrical with desired CS AASERTION DURATION OF 10 US. please look at attachment for the Screenshot&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Sun, 06 Dec 2020 20:48:35 GMT</pubDate>
    <dc:creator>hajianik</dc:creator>
    <dc:date>2020-12-06T20:48:35Z</dc:date>
    <item>
      <title>pcssck</title>
      <link>https://community.nxp.com/t5/S32K/pcssck/m-p/1194268#M9139</link>
      <description>&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Target is S32K148.&lt;/P&gt;&lt;P&gt;I'm trying to do an SPI transfer consisting of 5 bytes(40 bits) where the CS is asserted for the duration of transfer. The baud rate is &amp;nbsp;4mhz, peripheral Clock is PLL and Divider is 1 and peripheral Clock frequency is 40mhz , using SPI0 for this I have the following in LPSPI0_CCR:&lt;/P&gt;&lt;P&gt;SCKDIV 0X08&lt;/P&gt;&lt;P&gt;DBT 0X04&lt;/P&gt;&lt;P&gt;PCSSCK 0X03&lt;/P&gt;&lt;P&gt;SCKPCS 0X03&lt;/P&gt;&lt;P&gt;Using these values results in an uneven clock and longer CS assertion period. when I twig these parameters the clock changes but I am not able to achieve the desired symmetrical with desired CS AASERTION DURATION OF 10 US. please look at attachment for the Screenshot&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sun, 06 Dec 2020 20:48:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/pcssck/m-p/1194268#M9139</guid>
      <dc:creator>hajianik</dc:creator>
      <dc:date>2020-12-06T20:48:35Z</dc:date>
    </item>
    <item>
      <title>Re: pcssck</title>
      <link>https://community.nxp.com/t5/S32K/pcssck/m-p/1194733#M9146</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I understand the asymmetricity is in the SCK-to-PCS Delay / PCS-to-SCK Delay.&lt;/P&gt;
&lt;P&gt;But this can't be seen in the screenshot.&lt;/P&gt;
&lt;P&gt;Can you measure it with an oscilloscope and an active probe?&lt;/P&gt;
&lt;P&gt;Do you use the High-Drive pins? PCR[DSE] = 1.&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;S32K148 IO_Signal_Description_Input_Multiplexing.xlsx&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="danielmartynek_0-1607348153899.png" style="width: 563px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/131961i17467A1497ED6994/image-dimensions/563x176?v=v2" width="563" height="176" role="button" title="danielmartynek_0-1607348153899.png" alt="danielmartynek_0-1607348153899.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks,&lt;/P&gt;
&lt;P&gt;BR, Daniel&lt;/P&gt;</description>
      <pubDate>Mon, 07 Dec 2020 13:36:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/pcssck/m-p/1194733#M9146</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2020-12-07T13:36:49Z</dc:date>
    </item>
    <item>
      <title>Re: pcssck</title>
      <link>https://community.nxp.com/t5/S32K/pcssck/m-p/1194810#M9151</link>
      <description>&lt;P&gt;Hi Daniel,&lt;/P&gt;&lt;P&gt;Thanks for your quick response,&lt;/P&gt;&lt;P&gt;In the screen shot the clock(red color)&amp;nbsp;is not a%50 duty signal, Can't you see that?&lt;/P&gt;&lt;P&gt;when you say:&lt;/P&gt;&lt;P&gt;"I understand the asymmetricity is in the SCK-to-PCS Delay / PCS-to-SCK Delay"&lt;/P&gt;&lt;P&gt;You mean there are not the same?&lt;/P&gt;&lt;P&gt;Yes they are not the same.&lt;/P&gt;&lt;P&gt;I will measure it and I use hi drive pins for the clock signal and let you know.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Koorosh&lt;/P&gt;</description>
      <pubDate>Mon, 07 Dec 2020 15:58:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/pcssck/m-p/1194810#M9151</guid>
      <dc:creator>hajianik</dc:creator>
      <dc:date>2020-12-07T15:58:52Z</dc:date>
    </item>
    <item>
      <title>Re: pcssck</title>
      <link>https://community.nxp.com/t5/S32K/pcssck/m-p/1195465#M9171</link>
      <description>&lt;P&gt;Hi Koorosh,&lt;/P&gt;
&lt;P&gt;If you mean the 74.63% duty, it is not given by the SCK-to-PCS, PCS-to-SCK delays.&lt;/P&gt;
&lt;P&gt;For example, PCS-to-SCK is just the delay from the PCS assertion to the first SCK edge.&lt;/P&gt;
&lt;P&gt;The 35.6us delay is most likely caused by the CPU overhead.&lt;/P&gt;
&lt;P&gt;The SW must prepare another 40b transfer and it takes some time.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 08 Dec 2020 11:45:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/pcssck/m-p/1195465#M9171</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2020-12-08T11:45:15Z</dc:date>
    </item>
  </channel>
</rss>