<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic K118 Capture timer in S32K</title>
    <link>https://community.nxp.com/t5/S32K/K118-Capture-timer/m-p/1193191#M9108</link>
    <description>&lt;P&gt;Hello Mates,&amp;nbsp;&lt;/P&gt;&lt;P&gt;i'm looking to migrate a simple project for the K118 to the STM32 micro but need some help with the capture architecture. I need to read four square waves from 0 to 3KHz. In the STM32 two 16 bit timers are chained and a 10MHz clock is fed to the timers. The rising edge makes a interrupt to read the capture value. In the K118 can a timer have 4 interrupt capture channels?&lt;/P&gt;&lt;P&gt;Greetings, Renan&lt;/P&gt;</description>
    <pubDate>Thu, 03 Dec 2020 11:57:40 GMT</pubDate>
    <dc:creator>rvalente</dc:creator>
    <dc:date>2020-12-03T11:57:40Z</dc:date>
    <item>
      <title>K118 Capture timer</title>
      <link>https://community.nxp.com/t5/S32K/K118-Capture-timer/m-p/1193191#M9108</link>
      <description>&lt;P&gt;Hello Mates,&amp;nbsp;&lt;/P&gt;&lt;P&gt;i'm looking to migrate a simple project for the K118 to the STM32 micro but need some help with the capture architecture. I need to read four square waves from 0 to 3KHz. In the STM32 two 16 bit timers are chained and a 10MHz clock is fed to the timers. The rising edge makes a interrupt to read the capture value. In the K118 can a timer have 4 interrupt capture channels?&lt;/P&gt;&lt;P&gt;Greetings, Renan&lt;/P&gt;</description>
      <pubDate>Thu, 03 Dec 2020 11:57:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/K118-Capture-timer/m-p/1193191#M9108</guid>
      <dc:creator>rvalente</dc:creator>
      <dc:date>2020-12-03T11:57:40Z</dc:date>
    </item>
    <item>
      <title>Re: K118 Capture timer</title>
      <link>https://community.nxp.com/t5/S32K/K118-Capture-timer/m-p/1193348#M9115</link>
      <description>&lt;P&gt;Hello Renan,&lt;/P&gt;
&lt;P&gt;Each FTM channel can be configured for input capture.&lt;/P&gt;
&lt;P&gt;For more information, please take a look at the RM, Section 47.5.5 Input Capture Mode.&lt;/P&gt;
&lt;P&gt;You can use SDK, this example shows use of FTM Input capture: &lt;EM&gt;ftm_signal_measurement_s32k118&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;</description>
      <pubDate>Thu, 03 Dec 2020 15:38:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/K118-Capture-timer/m-p/1193348#M9115</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2020-12-03T15:38:42Z</dc:date>
    </item>
    <item>
      <title>Re: K118 Capture timer</title>
      <link>https://community.nxp.com/t5/S32K/K118-Capture-timer/m-p/1198933#M9242</link>
      <description>&lt;P&gt;Daniel,&lt;BR /&gt;&lt;BR /&gt;I can't see how to chain the FTMs to make a 32 bit timer capture, could you please give me a hint?&lt;/P&gt;</description>
      <pubDate>Mon, 14 Dec 2020 13:11:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/K118-Capture-timer/m-p/1198933#M9242</guid>
      <dc:creator>rvalente</dc:creator>
      <dc:date>2020-12-14T13:11:16Z</dc:date>
    </item>
    <item>
      <title>Re: K118 Capture timer</title>
      <link>https://community.nxp.com/t5/S32K/K118-Capture-timer/m-p/1199629#M9256</link>
      <description>&lt;P&gt;Daniel,&lt;BR /&gt;&lt;BR /&gt;how should I chain the FTM0 with FTM1 in K118 to make 32 bit ftm?&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm looking to feed a 1MHz clock to FTM1 so it'll overflow every 65ms, I want this overflow to increment FTM1, should I do this externally or can I internally route it?&lt;BR /&gt;&lt;BR /&gt;I believe Its fine to capture the FTM1 bits in software, so it would be set as a single counter only? Can I spare this timer and use another?&lt;/P&gt;</description>
      <pubDate>Tue, 15 Dec 2020 11:26:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/K118-Capture-timer/m-p/1199629#M9256</guid>
      <dc:creator>rvalente</dc:creator>
      <dc:date>2020-12-15T11:26:50Z</dc:date>
    </item>
  </channel>
</rss>