<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: multiple bit error and ECC function?</title>
    <link>https://community.nxp.com/t5/S32K/multiple-bit-error-and-ECC-function/m-p/1192855#M9094</link>
    <description>&lt;P&gt;Thanks luca,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;haw is error flag when multiple error occurred? (assume 4 bit) is that like double bit error?&lt;/P&gt;&lt;P&gt;B. assume we run DMA and it source address be a pointer to flash memory location (under 0x20000000), and destination address is an SRAM-U location. now we adjust DMA registers in a way that source address increments each time and source is fixed. can we use this method for finding error on flash ?&lt;/P&gt;&lt;P&gt;if Yes, is that good approach to test SRAM U &amp;amp; L, for finding errors before accessing the corrupt locations in runtime application?&lt;/P&gt;</description>
    <pubDate>Thu, 03 Dec 2020 05:09:36 GMT</pubDate>
    <dc:creator>JeorgeB</dc:creator>
    <dc:date>2020-12-03T05:09:36Z</dc:date>
    <item>
      <title>multiple bit error and ECC function?</title>
      <link>https://community.nxp.com/t5/S32K/multiple-bit-error-and-ECC-function/m-p/1190954#M9050</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;1 in s32k14x, ECC operates in Flash and SRAM memories and can detect single bit and dual bit error.&lt;/P&gt;&lt;P&gt;what happens if multiple bit error occurred in SRAM &amp;amp; Flash memories?&lt;/P&gt;&lt;P&gt;are they reported as dual bit error?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;2. is there any module like ERM for flash memory for showing the error address in flash memory?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Mon, 30 Nov 2020 13:33:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/multiple-bit-error-and-ECC-function/m-p/1190954#M9050</guid>
      <dc:creator>JeorgeB</dc:creator>
      <dc:date>2020-11-30T13:33:03Z</dc:date>
    </item>
    <item>
      <title>Re: multiple bit error and ECC function?</title>
      <link>https://community.nxp.com/t5/S32K/multiple-bit-error-and-ECC-function/m-p/1191632#M9066</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;we provide this application note which provides a lot of useful details related to this topic:&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN12522.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN12522.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The error is reported only when you access affected flash phrase – that means during data access or instruction fetch. So, you can get one error at a time. Next errors will be reported during next accesses.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Notice that Flash reports only double bit error. Single bit errors are automatically corrected and there’s no option to report it. Double bit error in flash triggers Bus Fault exception during data access or instruction fetch, so the failing flash address can be found in BFAR core register.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Lukas&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 01 Dec 2020 13:22:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/multiple-bit-error-and-ECC-function/m-p/1191632#M9066</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2020-12-01T13:22:25Z</dc:date>
    </item>
    <item>
      <title>Re: multiple bit error and ECC function?</title>
      <link>https://community.nxp.com/t5/S32K/multiple-bit-error-and-ECC-function/m-p/1192855#M9094</link>
      <description>&lt;P&gt;Thanks luca,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;haw is error flag when multiple error occurred? (assume 4 bit) is that like double bit error?&lt;/P&gt;&lt;P&gt;B. assume we run DMA and it source address be a pointer to flash memory location (under 0x20000000), and destination address is an SRAM-U location. now we adjust DMA registers in a way that source address increments each time and source is fixed. can we use this method for finding error on flash ?&lt;/P&gt;&lt;P&gt;if Yes, is that good approach to test SRAM U &amp;amp; L, for finding errors before accessing the corrupt locations in runtime application?&lt;/P&gt;</description>
      <pubDate>Thu, 03 Dec 2020 05:09:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/multiple-bit-error-and-ECC-function/m-p/1192855#M9094</guid>
      <dc:creator>JeorgeB</dc:creator>
      <dc:date>2020-12-03T05:09:36Z</dc:date>
    </item>
  </channel>
</rss>