<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 Eeprom initialization</title>
    <link>https://community.nxp.com/t5/S32K/Eeprom-initialization/m-p/1192236#M9079</link>
    <description>&lt;P&gt;Hello!&lt;BR /&gt;Initialization sometimes failed when I used EEPROM of S32K116, but after investigating and testing, I found that in debug mode, initialization could be successfully initialized if the break point stuck in the call initialization function.However, running directly to the end of initialization sometimes returns a failure.Please help me with this problem.&lt;BR /&gt;EEPROM initialization code is attached.&lt;BR /&gt;Thank you. Best wishes&lt;/P&gt;</description>
    <pubDate>Wed, 02 Dec 2020 09:54:27 GMT</pubDate>
    <dc:creator>972276616</dc:creator>
    <dc:date>2020-12-02T09:54:27Z</dc:date>
    <item>
      <title>Eeprom initialization</title>
      <link>https://community.nxp.com/t5/S32K/Eeprom-initialization/m-p/1192236#M9079</link>
      <description>&lt;P&gt;Hello!&lt;BR /&gt;Initialization sometimes failed when I used EEPROM of S32K116, but after investigating and testing, I found that in debug mode, initialization could be successfully initialized if the break point stuck in the call initialization function.However, running directly to the end of initialization sometimes returns a failure.Please help me with this problem.&lt;BR /&gt;EEPROM initialization code is attached.&lt;BR /&gt;Thank you. Best wishes&lt;/P&gt;</description>
      <pubDate>Wed, 02 Dec 2020 09:54:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Eeprom-initialization/m-p/1192236#M9079</guid>
      <dc:creator>972276616</dc:creator>
      <dc:date>2020-12-02T09:54:27Z</dc:date>
    </item>
    <item>
      <title>Re: Eeprom initialization</title>
      <link>https://community.nxp.com/t5/S32K/Eeprom-initialization/m-p/1192372#M9084</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Please make sure the function that launches the FTFC Program partition command is in SRAM.&lt;/P&gt;
&lt;P&gt;See the below threads.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32K/program-partition-command/m-p/1041468" target="_blank" rel="noopener"&gt;https://community.nxp.com/t5/S32K/program-partition-command/m-p/1041468&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32K/Linker-file-configuration-to-allow-code-execution-from-RAM/m-p/803493/highlight/true" target="_blank" rel="noopener"&gt;https://community.nxp.com/t5/S32K/Linker-file-configuration-to-allow-code-execution-from-RAM/m-p/803493/highlight/true&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;</description>
      <pubDate>Wed, 02 Dec 2020 13:37:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Eeprom-initialization/m-p/1192372#M9084</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2020-12-02T13:37:46Z</dc:date>
    </item>
    <item>
      <title>Re: Eeprom initialization</title>
      <link>https://community.nxp.com/t5/S32K/Eeprom-initialization/m-p/1193764#M9122</link>
      <description>&lt;P&gt;Hi,Daniel&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thank you very much for your help.Per your instructions, let me just put my EEPROM initialization function in RAM and execute it, as shown in the picture, shall I prefix the function with ___ (section(".code_ram"))?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Zhengyu&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 04 Dec 2020 07:43:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Eeprom-initialization/m-p/1193764#M9122</guid>
      <dc:creator>972276616</dc:creator>
      <dc:date>2020-12-04T07:43:18Z</dc:date>
    </item>
    <item>
      <title>Re: Eeprom initialization</title>
      <link>https://community.nxp.com/t5/S32K/Eeprom-initialization/m-p/1197175#M9194</link>
      <description>Hi,Daniel Thank you for your answer. I have one more question to ask you. When initialized in RAM, an EEPROM erases all Flash data. Regards, Zhengyu</description>
      <pubDate>Thu, 10 Dec 2020 07:37:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Eeprom-initialization/m-p/1197175#M9194</guid>
      <dc:creator>972276616</dc:creator>
      <dc:date>2020-12-10T07:37:13Z</dc:date>
    </item>
    <item>
      <title>Re: Eeprom initialization</title>
      <link>https://community.nxp.com/t5/S32K/Eeprom-initialization/m-p/1197177#M9195</link>
      <description>&lt;P&gt;Hi,Daniel Thank you for your answer. I have one more question to ask you. When initialized in RAM, an EEPROM erases all Flash data. Regards, Zhengyu&lt;/P&gt;</description>
      <pubDate>Thu, 10 Dec 2020 07:40:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Eeprom-initialization/m-p/1197177#M9195</guid>
      <dc:creator>972276616</dc:creator>
      <dc:date>2020-12-10T07:40:14Z</dc:date>
    </item>
    <item>
      <title>Re: Eeprom initialization</title>
      <link>https://community.nxp.com/t5/S32K/Eeprom-initialization/m-p/1197184#M9196</link>
      <description>&lt;P&gt;Hi,Daniel&lt;/P&gt;&lt;P&gt;Thank you for your answer. I have one more question to ask you. When initialized in RAM, an EEPROM erases all Flash data.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Zhengyu&lt;/P&gt;</description>
      <pubDate>Thu, 10 Dec 2020 07:43:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Eeprom-initialization/m-p/1197184#M9196</guid>
      <dc:creator>972276616</dc:creator>
      <dc:date>2020-12-10T07:43:41Z</dc:date>
    </item>
  </channel>
</rss>