<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic AN12218 UART bootloader problem in S32K</title>
    <link>https://community.nxp.com/t5/S32K/AN12218-UART-bootloader-problem/m-p/1188688#M8994</link>
    <description>&lt;P&gt;I can update one program, when update another program, it seems that the EVB can update the program, but the program does not work, it has confused me a few days, please help me, thanks!&lt;/P&gt;</description>
    <pubDate>Wed, 25 Nov 2020 07:26:14 GMT</pubDate>
    <dc:creator>wdong</dc:creator>
    <dc:date>2020-11-25T07:26:14Z</dc:date>
    <item>
      <title>AN12218 UART bootloader problem</title>
      <link>https://community.nxp.com/t5/S32K/AN12218-UART-bootloader-problem/m-p/1188688#M8994</link>
      <description>&lt;P&gt;I can update one program, when update another program, it seems that the EVB can update the program, but the program does not work, it has confused me a few days, please help me, thanks!&lt;/P&gt;</description>
      <pubDate>Wed, 25 Nov 2020 07:26:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/AN12218-UART-bootloader-problem/m-p/1188688#M8994</guid>
      <dc:creator>wdong</dc:creator>
      <dc:date>2020-11-25T07:26:14Z</dc:date>
    </item>
    <item>
      <title>Re: AN12218 UART bootloader problem</title>
      <link>https://community.nxp.com/t5/S32K/AN12218-UART-bootloader-problem/m-p/1189652#M9011</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Do you use your own project or example project?&lt;/P&gt;
&lt;P&gt;Can you share the .srec file and linker file of the project which does not work?&lt;/P&gt;
&lt;P&gt;You can check if the application is correctly loaded in the flash memory in the S32DS menu -&amp;gt; Window -&amp;gt; Show view -&amp;gt; Memory before the jump to the application.&lt;/P&gt;
&lt;P&gt;Do you have S32K148?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thank you.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Diana&lt;/P&gt;</description>
      <pubDate>Thu, 26 Nov 2020 10:17:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/AN12218-UART-bootloader-problem/m-p/1189652#M9011</guid>
      <dc:creator>dianabatrlova</dc:creator>
      <dc:date>2020-11-26T10:17:54Z</dc:date>
    </item>
    <item>
      <title>Re: AN12218 UART bootloader problem</title>
      <link>https://community.nxp.com/t5/S32K/AN12218-UART-bootloader-problem/m-p/1189984#M9018</link>
      <description>&lt;P&gt;hello, I used the example code, and now i have solved the problem.&lt;/P&gt;&lt;P&gt;Because the .srec file is not 8byte aligned which created by the S32DS, one must change the file&amp;nbsp;8byte aligned like use hex-view software.&lt;/P&gt;</description>
      <pubDate>Fri, 27 Nov 2020 02:40:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/AN12218-UART-bootloader-problem/m-p/1189984#M9018</guid>
      <dc:creator>wdong</dc:creator>
      <dc:date>2020-11-27T02:40:04Z</dc:date>
    </item>
  </channel>
</rss>