<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックTJA1145T/FD</title>
    <link>https://community.nxp.com/t5/S32K/TJA1145T-FD/m-p/1187998#M8969</link>
    <description>&lt;P&gt;Hi, noob here.&lt;/P&gt;&lt;P&gt;About TJA1145T/FD,I have a question:&lt;/P&gt;&lt;P&gt;I have refer to several designs with TJA1145T and I found that the 1145 communicates with microcontroller through SPI.If I follow the hardware design of 1145 but not send any SPI frame to&amp;nbsp;1145 when I power on the MCU board(In SW not initial the 1145),is the 1145 in operating mode or can MCU transmit and receive CAN frames by 1145?&lt;/P&gt;&lt;P&gt;I have code of a S32K application which uses UJA1169. However,there is no code about UJA1169 initial and SPI communication with microcontroller ,but it can still transfer CAN data.&lt;/P&gt;&lt;P&gt;You reply will be highly appreciated.Thanks.&lt;/P&gt;</description>
    <pubDate>Tue, 24 Nov 2020 08:40:30 GMT</pubDate>
    <dc:creator>carlos_kan</dc:creator>
    <dc:date>2020-11-24T08:40:30Z</dc:date>
    <item>
      <title>TJA1145T/FD</title>
      <link>https://community.nxp.com/t5/S32K/TJA1145T-FD/m-p/1187998#M8969</link>
      <description>&lt;P&gt;Hi, noob here.&lt;/P&gt;&lt;P&gt;About TJA1145T/FD,I have a question:&lt;/P&gt;&lt;P&gt;I have refer to several designs with TJA1145T and I found that the 1145 communicates with microcontroller through SPI.If I follow the hardware design of 1145 but not send any SPI frame to&amp;nbsp;1145 when I power on the MCU board(In SW not initial the 1145),is the 1145 in operating mode or can MCU transmit and receive CAN frames by 1145?&lt;/P&gt;&lt;P&gt;I have code of a S32K application which uses UJA1169. However,there is no code about UJA1169 initial and SPI communication with microcontroller ,but it can still transfer CAN data.&lt;/P&gt;&lt;P&gt;You reply will be highly appreciated.Thanks.&lt;/P&gt;</description>
      <pubDate>Tue, 24 Nov 2020 08:40:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/TJA1145T-FD/m-p/1187998#M8969</guid>
      <dc:creator>carlos_kan</dc:creator>
      <dc:date>2020-11-24T08:40:30Z</dc:date>
    </item>
    <item>
      <title>Re: TJA1145T/FD</title>
      <link>https://community.nxp.com/t5/S32K/TJA1145T-FD/m-p/1188978#M9006</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;upon power on TJA1145 enters Standby mode with CAN transceiver disabled, you need to send command over SPI. That is put TJA1145 in Normal mode (MC = 111) and enable CAN transceiver by setting bits CMC in the CAN control register to 01 or 10.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Wed, 25 Nov 2020 12:55:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/TJA1145T-FD/m-p/1188978#M9006</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2020-11-25T12:55:00Z</dc:date>
    </item>
    <item>
      <title>Re: TJA1145T/FD</title>
      <link>https://community.nxp.com/t5/S32K/TJA1145T-FD/m-p/2110151#M49565</link>
      <description>&lt;P&gt;&lt;FONT&gt;你好，我目前是使用S32K312向&lt;/FONT&gt;&lt;FONT&gt;&lt;FONT&gt;TJA1145T/FDJ发送SPI报文使其进入正常模式&lt;/FONT&gt;&lt;FONT&gt;&lt;FONT&gt;TJA1145T/FDJ的INH&lt;/FONT&gt;&lt;FONT&gt;&lt;FONT&gt;引脚电平是电源电压，但是CAN收发器依旧不能正常工作，是我的实现程序有问题吗，附件为我的实现程序，如方便请帮忙看看，谢谢#&lt;/FONT&gt;&lt;FONT&gt;TJA1145T/FDJ#S32K312&lt;/FONT&gt;&lt;/FONT&gt;&lt;/FONT&gt;&lt;/FONT&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 04 Jun 2025 07:19:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/TJA1145T-FD/m-p/2110151#M49565</guid>
      <dc:creator>Florence100733</dc:creator>
      <dc:date>2025-06-04T07:19:50Z</dc:date>
    </item>
  </channel>
</rss>