<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Receiving Ethernet Frames on S32K148 in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Receiving-Ethernet-Frames-on-S32K148/m-p/1186001#M8909</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm trying to read some frames with S32K148 EVB (176 pins) coming from an Arduino board (working at 150 MHz) via &lt;A href="https://technica-engineering.de/en/produkt/100base-t1-mediaconverter-bcm/" target="_self" rel="nofollow noopener noreferrer"&gt;media converter&lt;/A&gt; and &lt;A href="https://www.nxp.com/design/development-boards/analog-toolbox/tja1101-automotive-ethernet-adapter-for-s32k148evb-and-i-mx8:ADTJA1101-RMII" target="_self" rel="nofollow noopener noreferrer"&gt;TJA1101 daughter card&lt;/A&gt;. The demo application PHY TJA1101 in the SDK doesn't work as described in the application notes of the demo. The pre-integration of TJA110x driver is done as described in &lt;A href="https://www.nxp.com/docs/en/user-guide/ADTJA1101-RMIIUG.pdf" target="_self" rel="nofollow noopener noreferrer"&gt;ADTJA1101-RMII User Guide&lt;/A&gt;. The Ethernet component is configured to have RMII mode for data interface and it's 100 Mbps full-duplex. Each frame will have 4672 Bytes on the payload. The Processor Expert Code is generated before flashing the MCU with these settings. However, I can't get more than 48 valid (nonzero) Bytes at a time and those 48 Bytes don't have the values I set at Arduino side. Within those 48 Bytes, I can sometimes see the IP that I set at Arduino side and sometimes the data payload (of course inconsistent). What could the issue be here? You can find my main function and Arduino code attached. Any help would be appreciated.&lt;/P&gt;&lt;P&gt;Cheers,&lt;/P&gt;&lt;P&gt;Ozan&lt;/P&gt;</description>
    <pubDate>Thu, 19 Nov 2020 12:08:51 GMT</pubDate>
    <dc:creator>ozancs</dc:creator>
    <dc:date>2020-11-19T12:08:51Z</dc:date>
    <item>
      <title>Receiving Ethernet Frames on S32K148</title>
      <link>https://community.nxp.com/t5/S32K/Receiving-Ethernet-Frames-on-S32K148/m-p/1186001#M8909</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm trying to read some frames with S32K148 EVB (176 pins) coming from an Arduino board (working at 150 MHz) via &lt;A href="https://technica-engineering.de/en/produkt/100base-t1-mediaconverter-bcm/" target="_self" rel="nofollow noopener noreferrer"&gt;media converter&lt;/A&gt; and &lt;A href="https://www.nxp.com/design/development-boards/analog-toolbox/tja1101-automotive-ethernet-adapter-for-s32k148evb-and-i-mx8:ADTJA1101-RMII" target="_self" rel="nofollow noopener noreferrer"&gt;TJA1101 daughter card&lt;/A&gt;. The demo application PHY TJA1101 in the SDK doesn't work as described in the application notes of the demo. The pre-integration of TJA110x driver is done as described in &lt;A href="https://www.nxp.com/docs/en/user-guide/ADTJA1101-RMIIUG.pdf" target="_self" rel="nofollow noopener noreferrer"&gt;ADTJA1101-RMII User Guide&lt;/A&gt;. The Ethernet component is configured to have RMII mode for data interface and it's 100 Mbps full-duplex. Each frame will have 4672 Bytes on the payload. The Processor Expert Code is generated before flashing the MCU with these settings. However, I can't get more than 48 valid (nonzero) Bytes at a time and those 48 Bytes don't have the values I set at Arduino side. Within those 48 Bytes, I can sometimes see the IP that I set at Arduino side and sometimes the data payload (of course inconsistent). What could the issue be here? You can find my main function and Arduino code attached. Any help would be appreciated.&lt;/P&gt;&lt;P&gt;Cheers,&lt;/P&gt;&lt;P&gt;Ozan&lt;/P&gt;</description>
      <pubDate>Thu, 19 Nov 2020 12:08:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Receiving-Ethernet-Frames-on-S32K148/m-p/1186001#M8909</guid>
      <dc:creator>ozancs</dc:creator>
      <dc:date>2020-11-19T12:08:51Z</dc:date>
    </item>
    <item>
      <title>Re: Receiving Ethernet Frames on S32K148</title>
      <link>https://community.nxp.com/t5/S32K/Receiving-Ethernet-Frames-on-S32K148/m-p/1194896#M9153</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Did you also update maximum frame length in the Processor Expert configuration?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Veronica&lt;/P&gt;</description>
      <pubDate>Mon, 07 Dec 2020 17:23:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Receiving-Ethernet-Frames-on-S32K148/m-p/1194896#M9153</guid>
      <dc:creator>veronicavelciu</dc:creator>
      <dc:date>2020-12-07T17:23:40Z</dc:date>
    </item>
    <item>
      <title>Re: Receiving Ethernet Frames on S32K148</title>
      <link>https://community.nxp.com/t5/S32K/Receiving-Ethernet-Frames-on-S32K148/m-p/1194920#M9156</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/93284"&gt;@veronicavelciu&lt;/a&gt; ,&lt;/P&gt;&lt;P&gt;Yes I have, I set it to max. data length + 18 Bytes as recommended.&lt;/P&gt;&lt;P&gt;Cheers,&lt;/P&gt;&lt;P&gt;Ozan&lt;/P&gt;</description>
      <pubDate>Mon, 07 Dec 2020 18:29:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Receiving-Ethernet-Frames-on-S32K148/m-p/1194920#M9156</guid>
      <dc:creator>ozancs</dc:creator>
      <dc:date>2020-12-07T18:29:01Z</dc:date>
    </item>
    <item>
      <title>Re: Receiving Ethernet Frames on S32K148</title>
      <link>https://community.nxp.com/t5/S32K/Receiving-Ethernet-Frames-on-S32K148/m-p/1204156#M9389</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/178292"&gt;@ozancs&lt;/a&gt;&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;Can you provide the configuration of your application?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;Cuong&lt;/P&gt;</description>
      <pubDate>Thu, 24 Dec 2020 15:31:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Receiving-Ethernet-Frames-on-S32K148/m-p/1204156#M9389</guid>
      <dc:creator>cuongnguyenvan</dc:creator>
      <dc:date>2020-12-24T15:31:26Z</dc:date>
    </item>
    <item>
      <title>Re: Receiving Ethernet Frames on S32K148</title>
      <link>https://community.nxp.com/t5/S32K/Receiving-Ethernet-Frames-on-S32K148/m-p/1252570#M10324</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/178292"&gt;@ozancs&lt;/a&gt; ,&lt;/P&gt;
&lt;P&gt;Do you still have th&lt;FONT style="background-color: #ffffff;"&gt;is&lt;/FONT&gt;&amp;nbsp;&lt;FONT style="background-color: #ffffff;"&gt;is&lt;/FONT&gt;sue?&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Vu&lt;/P&gt;</description>
      <pubDate>Fri, 26 Mar 2021 04:37:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Receiving-Ethernet-Frames-on-S32K148/m-p/1252570#M10324</guid>
      <dc:creator>vutran</dc:creator>
      <dc:date>2021-03-26T04:37:02Z</dc:date>
    </item>
  </channel>
</rss>