<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 Re: S32K144EVAL</title>
    <link>https://community.nxp.com/t5/S32K/S32K144EVAL/m-p/676950#M870</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the response.&lt;/P&gt;&lt;P&gt;The debugger view is displayed however no source ,no registers, no variable , nothing can be read.&lt;/P&gt;&lt;P&gt;It is not running correctly. I looked at reset pin on scope and it looks like&amp;nbsp; a watchdog reset every 8 ms or so , reset is triggered.&lt;/P&gt;&lt;P&gt;I don't think it is a watchdog reset though, It is more like a running reset.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Koorosh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 15 May 2017 20:53:10 GMT</pubDate>
    <dc:creator>hajianik</dc:creator>
    <dc:date>2017-05-15T20:53:10Z</dc:date>
    <item>
      <title>S32K144EVAL</title>
      <link>https://community.nxp.com/t5/S32K/S32K144EVAL/m-p/676948#M868</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;When I power the S32K144EVAL board via micro USB cable or externally via 12v power supply ,The LED next to the reset button is on and a bit dim and I can't do anything such as flash/debug. Does this mean the board is in a reset state?&lt;/P&gt;&lt;P&gt;I'm using S32 Design studio.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any Ideas?&lt;/P&gt;&lt;P&gt;Koorosh Hajiani&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 May 2017 15:49:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144EVAL/m-p/676948#M868</guid>
      <dc:creator>hajianik</dc:creator>
      <dc:date>2017-05-11T15:49:46Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144EVAL</title>
      <link>https://community.nxp.com/t5/S32K/S32K144EVAL/m-p/676949#M869</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Are you able to just attach the debugger to the running MCU and look at registers?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/18151i75F121416D34DD1D/image-size/large?v=v2&amp;amp;px=999" title="attach_to_running_target.png" alt="attach_to_running_target.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 May 2017 18:54:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144EVAL/m-p/676949#M869</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2017-05-15T18:54:02Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144EVAL</title>
      <link>https://community.nxp.com/t5/S32K/S32K144EVAL/m-p/676950#M870</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the response.&lt;/P&gt;&lt;P&gt;The debugger view is displayed however no source ,no registers, no variable , nothing can be read.&lt;/P&gt;&lt;P&gt;It is not running correctly. I looked at reset pin on scope and it looks like&amp;nbsp; a watchdog reset every 8 ms or so , reset is triggered.&lt;/P&gt;&lt;P&gt;I don't think it is a watchdog reset though, It is more like a running reset.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Koorosh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 May 2017 20:53:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144EVAL/m-p/676950#M870</guid>
      <dc:creator>hajianik</dc:creator>
      <dc:date>2017-05-15T20:53:10Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144EVAL</title>
      <link>https://community.nxp.com/t5/S32K/S32K144EVAL/m-p/676951#M871</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I assume this is the issue we discussed in thread&amp;nbsp;&lt;A _jive_internal="true" href="https://community.nxp.com/thread/451040"&gt;S32k open sda secure flash issue.&lt;/A&gt; &lt;/P&gt;&lt;P&gt;Unfortunately, I still don’t have a solution.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 May 2017 18:33:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144EVAL/m-p/676951#M871</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2017-05-18T18:33:12Z</dc:date>
    </item>
  </channel>
</rss>