<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Ethernet MDIO driver in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Ethernet-MDIO-driver/m-p/1178567#M8699</link>
    <description>&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;I have a board where only the Ethernet MDC and MDIO lines are connected to S32K148 controller and the data lines are connected to a different application processor. The S32K controller is supposed to only initialize the PHY.&lt;/P&gt;&lt;P&gt;For this I am looking for a sample MDIO driver, that can be used for setting up only the MDC clock and read/write over MDIO interface.&lt;/P&gt;&lt;P&gt;I couldn't find any such example codes in S32DS. Can someone please help with this?&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Guru&lt;/P&gt;</description>
    <pubDate>Thu, 05 Nov 2020 06:59:49 GMT</pubDate>
    <dc:creator>sgp_118</dc:creator>
    <dc:date>2020-11-05T06:59:49Z</dc:date>
    <item>
      <title>Ethernet MDIO driver</title>
      <link>https://community.nxp.com/t5/S32K/Ethernet-MDIO-driver/m-p/1178567#M8699</link>
      <description>&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;I have a board where only the Ethernet MDC and MDIO lines are connected to S32K148 controller and the data lines are connected to a different application processor. The S32K controller is supposed to only initialize the PHY.&lt;/P&gt;&lt;P&gt;For this I am looking for a sample MDIO driver, that can be used for setting up only the MDC clock and read/write over MDIO interface.&lt;/P&gt;&lt;P&gt;I couldn't find any such example codes in S32DS. Can someone please help with this?&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Guru&lt;/P&gt;</description>
      <pubDate>Thu, 05 Nov 2020 06:59:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Ethernet-MDIO-driver/m-p/1178567#M8699</guid>
      <dc:creator>sgp_118</dc:creator>
      <dc:date>2020-11-05T06:59:49Z</dc:date>
    </item>
    <item>
      <title>Re: Ethernet MDIO driver</title>
      <link>https://community.nxp.com/t5/S32K/Ethernet-MDIO-driver/m-p/1179989#M8728</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;what about "phy_tja1101_s32k148" demo example. Could this be helpful?&lt;/P&gt;
&lt;P&gt;It shows MDIO communication with TJA1101.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 09 Nov 2020 08:49:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Ethernet-MDIO-driver/m-p/1179989#M8728</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2020-11-09T08:49:40Z</dc:date>
    </item>
    <item>
      <title>Re: Ethernet MDIO driver</title>
      <link>https://community.nxp.com/t5/S32K/Ethernet-MDIO-driver/m-p/1180822#M8766</link>
      <description>&lt;P&gt;Thanks Petr.&lt;/P&gt;</description>
      <pubDate>Tue, 10 Nov 2020 14:00:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Ethernet-MDIO-driver/m-p/1180822#M8766</guid>
      <dc:creator>sgp_118</dc:creator>
      <dc:date>2020-11-10T14:00:08Z</dc:date>
    </item>
  </channel>
</rss>