<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32Kのトピックsoftware reset for S32K144</title>
    <link>https://community.nxp.com/t5/S32K/software-reset-for-S32K144/m-p/1176802#M8657</link>
    <description>&lt;P&gt;I am creating a bootloader code. here my bootloader code is in d-flash (0x10000000). Here the VTOR is in p-flash only (0x00000000 - 0x00000410). I'm writing my application via bootloader on 0x00002000 location where VTOR for application is at 0x00002000 - 0x00002410 &amp;amp; actual text starts after 0x00002410. After jumping from bootloader to application, I'm waiting for certain commands there, and when I get that command, I'll jump back to the bootloader code with a software reset. Please explain to me a way to do a software reset. Currently, I'm using&amp;nbsp;SystemSoftwareReset() given in system_S32K144.c&lt;SPAN&gt;, but after resetting and jumping back to bootloader code, it directly goes to default ISR instead of running the main code there. If I keep the entire bootloader code at 0x00000000, including text which previously I was keeping at 0x10000000 location, then it will work; otherwise, this software reset is not working for me.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Please help me to figure out how to handle this software reset. I appreciate any help you can provide. &lt;LI-EMOJI id="lia_slightly-smiling-face" title=":slightly_smiling_face:"&gt;&lt;/LI-EMOJI&gt;&lt;/P&gt;</description>
    <pubDate>Mon, 02 Nov 2020 20:02:01 GMT</pubDate>
    <dc:creator>d_shivamkumar</dc:creator>
    <dc:date>2020-11-02T20:02:01Z</dc:date>
    <item>
      <title>software reset for S32K144</title>
      <link>https://community.nxp.com/t5/S32K/software-reset-for-S32K144/m-p/1176802#M8657</link>
      <description>&lt;P&gt;I am creating a bootloader code. here my bootloader code is in d-flash (0x10000000). Here the VTOR is in p-flash only (0x00000000 - 0x00000410). I'm writing my application via bootloader on 0x00002000 location where VTOR for application is at 0x00002000 - 0x00002410 &amp;amp; actual text starts after 0x00002410. After jumping from bootloader to application, I'm waiting for certain commands there, and when I get that command, I'll jump back to the bootloader code with a software reset. Please explain to me a way to do a software reset. Currently, I'm using&amp;nbsp;SystemSoftwareReset() given in system_S32K144.c&lt;SPAN&gt;, but after resetting and jumping back to bootloader code, it directly goes to default ISR instead of running the main code there. If I keep the entire bootloader code at 0x00000000, including text which previously I was keeping at 0x10000000 location, then it will work; otherwise, this software reset is not working for me.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Please help me to figure out how to handle this software reset. I appreciate any help you can provide. &lt;LI-EMOJI id="lia_slightly-smiling-face" title=":slightly_smiling_face:"&gt;&lt;/LI-EMOJI&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 02 Nov 2020 20:02:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/software-reset-for-S32K144/m-p/1176802#M8657</guid>
      <dc:creator>d_shivamkumar</dc:creator>
      <dc:date>2020-11-02T20:02:01Z</dc:date>
    </item>
    <item>
      <title>Re: software reset for S32K144</title>
      <link>https://community.nxp.com/t5/S32K/software-reset-for-S32K144/m-p/1185477#M8890</link>
      <description>&lt;P&gt;Hello&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I suggest you refer to AN12218 &lt;A href="https://www.nxp.com/docs/en/application-note/AN12218.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN12218.pdf&lt;/A&gt;. Also, you can find an example of this application at AN12218SW.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Let me know if this is helpful, if you have more questions do not hesitate to ask me.&lt;/P&gt;</description>
      <pubDate>Wed, 18 Nov 2020 20:52:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/software-reset-for-S32K144/m-p/1185477#M8890</guid>
      <dc:creator>Omar_Anguiano</dc:creator>
      <dc:date>2020-11-18T20:52:21Z</dc:date>
    </item>
  </channel>
</rss>