<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Recoverin JTAG lines to default state in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Recoverin-JTAG-lines-to-default-state/m-p/1176210#M8635</link>
    <description>&lt;P&gt;Hello Robin&lt;/P&gt;&lt;P&gt;thanks for sharing the software.&lt;/P&gt;&lt;P&gt;I have tried with the shared software, it too did not work for me.&lt;/P&gt;&lt;P&gt;Thinking to cross check the hardware setup I have for the custom board, will diagnoses and reply back.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Jayakumar Appari.&lt;/P&gt;</description>
    <pubDate>Sun, 01 Nov 2020 05:33:20 GMT</pubDate>
    <dc:creator>jaikumar81</dc:creator>
    <dc:date>2020-11-01T05:33:20Z</dc:date>
    <item>
      <title>Recoverin JTAG lines to default state</title>
      <link>https://community.nxp.com/t5/S32K/Recoverin-JTAG-lines-to-default-state/m-p/1173644#M8586</link>
      <description>&lt;P&gt;Dear Team&lt;/P&gt;&lt;P&gt;We noticed there was some problem in port initialization(of Autosar configuration) due to which controller (S32k148-100 pin) is resetting.&lt;/P&gt;&lt;P&gt;To analyze the same and zero down further we have started deactivating few ports(probably deactivated even JTAG lines too).&amp;nbsp;&lt;/P&gt;&lt;P&gt;Due to the above reason, now we are unable to flash the image using S32kDesign studio using PnE debugger. I&amp;nbsp;have attached snapshot of the same.&lt;/P&gt;&lt;P&gt;Kindly share the inputs, how JTAG lines could be recovered to its default state.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Jayakumar Appari.&lt;/P&gt;</description>
      <pubDate>Tue, 27 Oct 2020 07:47:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Recoverin-JTAG-lines-to-default-state/m-p/1173644#M8586</guid>
      <dc:creator>jaikumar81</dc:creator>
      <dc:date>2020-10-27T07:47:18Z</dc:date>
    </item>
    <item>
      <title>Re: Recoverin JTAG lines to default state</title>
      <link>https://community.nxp.com/t5/S32K/Recoverin-JTAG-lines-to-default-state/m-p/1173674#M8587</link>
      <description>&lt;P&gt;Hi&amp;nbsp;jaikumar81,&lt;/P&gt;
&lt;P&gt;Please try to use the &lt;STRONG&gt;P&amp;amp;E Recovery Utility&lt;/STRONG&gt; described in "&lt;A href="https://mcuoneclipse.com/2013/06/16/bricking-and-recovering-frdm-kl25z-boards-reset-swd-clock-and-low-power/" target="_self"&gt;Bricking and Recovering FRDM-KL25Z Boards: Reset, SWD Clock and Low Power&lt;/A&gt;".&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Tue, 27 Oct 2020 08:24:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Recoverin-JTAG-lines-to-default-state/m-p/1173674#M8587</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2020-10-27T08:24:54Z</dc:date>
    </item>
    <item>
      <title>Re: Recoverin JTAG lines to default state</title>
      <link>https://community.nxp.com/t5/S32K/Recoverin-JTAG-lines-to-default-state/m-p/1173827#M8589</link>
      <description>&lt;P&gt;Hello Robin,&lt;/P&gt;&lt;P&gt;thanks for sharing the supporting link.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have tried couple of retries(S32k148-100, custom board) with Kinetis_Recovery_Utility , and has following error "could not place the controller in halt state", when connected to the target with PnE debugher (using USB Multi Link)&lt;/P&gt;&lt;P&gt;To verify whether&amp;nbsp;Kinetis_Recovery_Utility is actually testable on S32K, I have tried with S32k148-144(eval board) in openSD mode.&lt;/P&gt;&lt;P&gt;However with eval board too, I have same error "could not place the controller in halt state".&lt;/P&gt;&lt;P&gt;I am expecting this(Kinetis_Recovery_Utility) should have worked atleast on eval board.&lt;/P&gt;&lt;P&gt;There are no issues in connecting to eval board(in OpenSd mode) and also with PnE debuger,&amp;nbsp; I could connect other custom board (S32k!48-100)too.&lt;/P&gt;&lt;P&gt;Kindly let me know, if there is any other means to change the default state of JTAG lines.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Jayakumar Appari.&lt;/P&gt;</description>
      <pubDate>Tue, 27 Oct 2020 11:54:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Recoverin-JTAG-lines-to-default-state/m-p/1173827#M8589</guid>
      <dc:creator>jaikumar81</dc:creator>
      <dc:date>2020-10-27T11:54:59Z</dc:date>
    </item>
    <item>
      <title>Re: Recoverin JTAG lines to default state</title>
      <link>https://community.nxp.com/t5/S32K/Recoverin-JTAG-lines-to-default-state/m-p/1174406#M8605</link>
      <description>&lt;P&gt;When I use the old version of&amp;nbsp;&lt;STRONG&gt;Kinetis_Recovery_Utility&lt;/STRONG&gt;, it was able to halt it.(on board OpenSDA of S32K148EVB and external P&amp;amp;E Multilink RevB )&lt;BR /&gt;But when use the latest version&amp;nbsp;Kinetis_Recovery_Utility, it does not work.&lt;BR /&gt;I have attached the old version of&amp;nbsp;Kinetis_Recovery_Utility.&lt;/P&gt;</description>
      <pubDate>Wed, 28 Oct 2020 09:11:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Recoverin-JTAG-lines-to-default-state/m-p/1174406#M8605</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2020-10-28T09:11:50Z</dc:date>
    </item>
    <item>
      <title>Re: Recoverin JTAG lines to default state</title>
      <link>https://community.nxp.com/t5/S32K/Recoverin-JTAG-lines-to-default-state/m-p/1176210#M8635</link>
      <description>&lt;P&gt;Hello Robin&lt;/P&gt;&lt;P&gt;thanks for sharing the software.&lt;/P&gt;&lt;P&gt;I have tried with the shared software, it too did not work for me.&lt;/P&gt;&lt;P&gt;Thinking to cross check the hardware setup I have for the custom board, will diagnoses and reply back.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Jayakumar Appari.&lt;/P&gt;</description>
      <pubDate>Sun, 01 Nov 2020 05:33:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Recoverin-JTAG-lines-to-default-state/m-p/1176210#M8635</guid>
      <dc:creator>jaikumar81</dc:creator>
      <dc:date>2020-11-01T05:33:20Z</dc:date>
    </item>
  </channel>
</rss>