<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Run code immediately on reset without starting debug (S32K116 evaluation board) in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Run-code-immediately-on-reset-without-starting-debug-S32K116/m-p/1175258#M8614</link>
    <description>&lt;P&gt;Hi, my code on the evaluation board doesn't run when I power on the board (via OpenSDA on USB): I have to start debugging to run the code. How can I set the board to run the code always when powered (even with external power supply, without connecting to the USB)?&lt;/P&gt;</description>
    <pubDate>Thu, 29 Oct 2020 11:35:25 GMT</pubDate>
    <dc:creator>Drifter22</dc:creator>
    <dc:date>2020-10-29T11:35:25Z</dc:date>
    <item>
      <title>Run code immediately on reset without starting debug (S32K116 evaluation board)</title>
      <link>https://community.nxp.com/t5/S32K/Run-code-immediately-on-reset-without-starting-debug-S32K116/m-p/1175258#M8614</link>
      <description>&lt;P&gt;Hi, my code on the evaluation board doesn't run when I power on the board (via OpenSDA on USB): I have to start debugging to run the code. How can I set the board to run the code always when powered (even with external power supply, without connecting to the USB)?&lt;/P&gt;</description>
      <pubDate>Thu, 29 Oct 2020 11:35:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Run-code-immediately-on-reset-without-starting-debug-S32K116/m-p/1175258#M8614</guid>
      <dc:creator>Drifter22</dc:creator>
      <dc:date>2020-10-29T11:35:25Z</dc:date>
    </item>
    <item>
      <title>Re: Run code immediately on reset without starting debug (S32K116 evaluation board)</title>
      <link>https://community.nxp.com/t5/S32K/Run-code-immediately-on-reset-without-starting-debug-S32K116/m-p/1175766#M8622</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Please make sure code is in the Flash not SRAM.&lt;/P&gt;
&lt;P&gt;You can power the board via the 12V connector, you need to change J107 to position 1-2.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="danielmartynek_0-1604046048473.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/128695i0DFD87A6D4CC9601/image-size/medium?v=v2&amp;amp;px=400" role="button" title="danielmartynek_0-1604046048473.png" alt="danielmartynek_0-1604046048473.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;danielmartynek_0-1604046048473.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 30 Oct 2020 08:21:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Run-code-immediately-on-reset-without-starting-debug-S32K116/m-p/1175766#M8622</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2020-10-30T08:21:13Z</dc:date>
    </item>
  </channel>
</rss>