<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: S32K146 Passive Filter Enable function</title>
    <link>https://community.nxp.com/t5/S32K/S32K146-Passive-Filter-Enable-function/m-p/1172282#M8562</link>
    <description>&lt;P&gt;Hi&amp;nbsp;kkw,&lt;/P&gt;
&lt;P&gt;Please refer &lt;STRONG&gt;S32K146_IO_Signal_Description_Input_Multiplexing.xlsx&lt;/STRONG&gt; that is attached to the S32K-RM.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="S32K-RM.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/128113i4597957CDEE867B9/image-size/large?v=v2&amp;amp;px=999" role="button" title="S32K-RM.png" alt="S32K-RM.png" /&gt;&lt;/span&gt;&lt;BR /&gt;In IO Signal Table, column &lt;STRONG&gt;U&lt;/STRONG&gt; shows the reset state of PCR_PFE (bit 4) and column &lt;STRONG&gt;V&lt;/STRONG&gt; specifies which pin has the PFE bit configurable.&lt;BR /&gt;Unfortunately PTC15 does not support this feature.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="S32K146_IO_Signal_Description_Input_Multiplexing.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/128114i27FC629647F3A782/image-size/large?v=v2&amp;amp;px=999" role="button" title="S32K146_IO_Signal_Description_Input_Multiplexing.png" alt="S32K146_IO_Signal_Description_Input_Multiplexing.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
    <pubDate>Fri, 23 Oct 2020 07:46:23 GMT</pubDate>
    <dc:creator>Robin_Shen</dc:creator>
    <dc:date>2020-10-23T07:46:23Z</dc:date>
    <item>
      <title>S32K146 Passive Filter Enable function</title>
      <link>https://community.nxp.com/t5/S32K/S32K146-Passive-Filter-Enable-function/m-p/1172174#M8560</link>
      <description>&lt;P&gt;Hi:&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; I used PTC15 as GPIO function, set input mode with pulldown register and enable&amp;nbsp; Passive Filter . Then connect 1 HZ, 1KHZ, 1MHZ, 30 MHZ, 50 MHZ&amp;nbsp;square wave&amp;nbsp; to PTC15. But PTC 15 can detect high.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;Will Passive Filter function filter high frenquency? Why PTC15 can detect high level? Is all GPIO has this fucntion?&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 23 Oct 2020 04:04:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K146-Passive-Filter-Enable-function/m-p/1172174#M8560</guid>
      <dc:creator>kkw</dc:creator>
      <dc:date>2020-10-23T04:04:14Z</dc:date>
    </item>
    <item>
      <title>Re: S32K146 Passive Filter Enable function</title>
      <link>https://community.nxp.com/t5/S32K/S32K146-Passive-Filter-Enable-function/m-p/1172282#M8562</link>
      <description>&lt;P&gt;Hi&amp;nbsp;kkw,&lt;/P&gt;
&lt;P&gt;Please refer &lt;STRONG&gt;S32K146_IO_Signal_Description_Input_Multiplexing.xlsx&lt;/STRONG&gt; that is attached to the S32K-RM.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="S32K-RM.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/128113i4597957CDEE867B9/image-size/large?v=v2&amp;amp;px=999" role="button" title="S32K-RM.png" alt="S32K-RM.png" /&gt;&lt;/span&gt;&lt;BR /&gt;In IO Signal Table, column &lt;STRONG&gt;U&lt;/STRONG&gt; shows the reset state of PCR_PFE (bit 4) and column &lt;STRONG&gt;V&lt;/STRONG&gt; specifies which pin has the PFE bit configurable.&lt;BR /&gt;Unfortunately PTC15 does not support this feature.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="S32K146_IO_Signal_Description_Input_Multiplexing.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/128114i27FC629647F3A782/image-size/large?v=v2&amp;amp;px=999" role="button" title="S32K146_IO_Signal_Description_Input_Multiplexing.png" alt="S32K146_IO_Signal_Description_Input_Multiplexing.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Fri, 23 Oct 2020 07:46:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K146-Passive-Filter-Enable-function/m-p/1172282#M8562</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2020-10-23T07:46:23Z</dc:date>
    </item>
  </channel>
</rss>