<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Code Flash issue for S32K2TV eval kit in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Code-Flash-issue-for-S32K2TV-eval-kit/m-p/1167199#M8476</link>
    <description>&lt;P&gt;Hello ,&lt;/P&gt;&lt;P&gt;I have been using S32K2TV EVAL kit for development puposes but recently facing issues related to flashing of code to it. Once i used handwritten code to flash and debug through OSDA and was successful to do so but later we switched to EB Generated code for the micro. After flashing the EB generated micro i was not able to debug the code and hence decided to switch back to handwritten code as suggest by NXP. Now the issue is that ater that day i am not able to flash even a simple hand written LED code to it. An error "Error in service launch sequence" pops up everytime i have even checked all debug configuration setting there i am able to detect the debugger but could't flash it. I cannot understand the issue and would request help.&lt;/P&gt;</description>
    <pubDate>Wed, 14 Oct 2020 06:34:43 GMT</pubDate>
    <dc:creator>manish_dev</dc:creator>
    <dc:date>2020-10-14T06:34:43Z</dc:date>
    <item>
      <title>Code Flash issue for S32K2TV eval kit</title>
      <link>https://community.nxp.com/t5/S32K/Code-Flash-issue-for-S32K2TV-eval-kit/m-p/1167199#M8476</link>
      <description>&lt;P&gt;Hello ,&lt;/P&gt;&lt;P&gt;I have been using S32K2TV EVAL kit for development puposes but recently facing issues related to flashing of code to it. Once i used handwritten code to flash and debug through OSDA and was successful to do so but later we switched to EB Generated code for the micro. After flashing the EB generated micro i was not able to debug the code and hence decided to switch back to handwritten code as suggest by NXP. Now the issue is that ater that day i am not able to flash even a simple hand written LED code to it. An error "Error in service launch sequence" pops up everytime i have even checked all debug configuration setting there i am able to detect the debugger but could't flash it. I cannot understand the issue and would request help.&lt;/P&gt;</description>
      <pubDate>Wed, 14 Oct 2020 06:34:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Code-Flash-issue-for-S32K2TV-eval-kit/m-p/1167199#M8476</guid>
      <dc:creator>manish_dev</dc:creator>
      <dc:date>2020-10-14T06:34:43Z</dc:date>
    </item>
  </channel>
</rss>