<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックUsing S32K148EVB as Flasher/Debugger for external S32K148 based custom hardware using OpenSDA</title>
    <link>https://community.nxp.com/t5/S32K/Using-S32K148EVB-as-Flasher-Debugger-for-external-S32K148-based/m-p/1165645#M8441</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;After going through the schematic for the said EVB (S32K148EVB-SCH-29644-RB.pdf), we find that the EVB 'can be' used to Flash/Debug a S32K148 based external custom hardware, through J20 connector and managing 'Isolation Resistors'&lt;/P&gt;&lt;P&gt;But there is no specific mention of this facility either in Quick Start Guide (S32K148EVB-QSG.pdf) or User Manual (S32K148-UM.pdf).&lt;/P&gt;&lt;P&gt;Can somebody confirm this and if yes, with what modifications.&lt;/P&gt;&lt;P&gt;We intend to use the EVB that is available with us for this intended application for our new project based on S32K148.&lt;/P&gt;&lt;P&gt;Thank you very much&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;- Vijay Vaidya&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Sun, 11 Oct 2020 13:16:54 GMT</pubDate>
    <dc:creator>vijayvaidya</dc:creator>
    <dc:date>2020-10-11T13:16:54Z</dc:date>
    <item>
      <title>Using S32K148EVB as Flasher/Debugger for external S32K148 based custom hardware using OpenSDA</title>
      <link>https://community.nxp.com/t5/S32K/Using-S32K148EVB-as-Flasher-Debugger-for-external-S32K148-based/m-p/1165645#M8441</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;After going through the schematic for the said EVB (S32K148EVB-SCH-29644-RB.pdf), we find that the EVB 'can be' used to Flash/Debug a S32K148 based external custom hardware, through J20 connector and managing 'Isolation Resistors'&lt;/P&gt;&lt;P&gt;But there is no specific mention of this facility either in Quick Start Guide (S32K148EVB-QSG.pdf) or User Manual (S32K148-UM.pdf).&lt;/P&gt;&lt;P&gt;Can somebody confirm this and if yes, with what modifications.&lt;/P&gt;&lt;P&gt;We intend to use the EVB that is available with us for this intended application for our new project based on S32K148.&lt;/P&gt;&lt;P&gt;Thank you very much&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;- Vijay Vaidya&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sun, 11 Oct 2020 13:16:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Using-S32K148EVB-as-Flasher-Debugger-for-external-S32K148-based/m-p/1165645#M8441</guid>
      <dc:creator>vijayvaidya</dc:creator>
      <dc:date>2020-10-11T13:16:54Z</dc:date>
    </item>
    <item>
      <title>Re: Using S32K148EVB as Flasher/Debugger for external S32K148 based custom hardware using OpenSDA</title>
      <link>https://community.nxp.com/t5/S32K/Using-S32K148EVB-as-Flasher-Debugger-for-external-S32K148-based/m-p/1165937#M8447</link>
      <description>&lt;P&gt;I'm afraid it can not achieve.&lt;/P&gt;
&lt;P&gt;You can refer this:&amp;nbsp;&lt;A href="https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-t-flash-elf-to-S32K146Q100-by-OpenSDA/m-p/1007289" target="_self"&gt;Can't flash elf to S32K146Q100 by OpenSDA&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Robin&lt;/P&gt;
&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Mon, 12 Oct 2020 08:25:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Using-S32K148EVB-as-Flasher-Debugger-for-external-S32K148-based/m-p/1165937#M8447</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2020-10-12T08:25:29Z</dc:date>
    </item>
    <item>
      <title>Re: Using S32K148EVB as Flasher/Debugger for external S32K148 based custom hardware using OpenSDA</title>
      <link>https://community.nxp.com/t5/S32K/Using-S32K148EVB-as-Flasher-Debugger-for-external-S32K148-based/m-p/1166041#M8449</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Thanks Robin_Shen for your inputs.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;- Vijay Vaidya&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 12 Oct 2020 12:05:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Using-S32K148EVB-as-Flasher-Debugger-for-external-S32K148-based/m-p/1166041#M8449</guid>
      <dc:creator>vijayvaidya</dc:creator>
      <dc:date>2020-10-12T12:05:41Z</dc:date>
    </item>
  </channel>
</rss>