<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Processor Expert for S32DS for ARM in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Processor-Expert-for-S32DS-for-ARM/m-p/1164540#M8425</link>
    <description>&lt;P&gt;I have a problem with processor expert and generated code.&lt;/P&gt;&lt;P&gt;I add the PinSettings component to my project and configured needed pins. In the folder “Generated Code” I can see the file pin_mux with corresponding structures. But I can not find the way, how I can add the automatic initialization function to my main.c file. The same for other components.&lt;/P&gt;&lt;P&gt;The HELP says „&lt;FONT face="Times New Roman, serif"&gt;&lt;FONT size="3"&gt;You can let Processor Expert call the Init method automatically by selecting "yes" for the Call Init method in the Initialization group of the Component's properties. „ &lt;/FONT&gt;&lt;/FONT&gt;&lt;FONT face="Times New Roman, serif"&gt;&lt;FONT size="3"&gt;But there is no such setting by me. &lt;/FONT&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Times New Roman, serif"&gt;&lt;FONT size="3"&gt;Thank you very much for your help!&lt;/FONT&gt;&lt;/FONT&gt;&lt;/P&gt;</description>
    <pubDate>Thu, 08 Oct 2020 13:21:19 GMT</pubDate>
    <dc:creator>DenisT1980</dc:creator>
    <dc:date>2020-10-08T13:21:19Z</dc:date>
    <item>
      <title>Processor Expert for S32DS for ARM</title>
      <link>https://community.nxp.com/t5/S32K/Processor-Expert-for-S32DS-for-ARM/m-p/1164540#M8425</link>
      <description>&lt;P&gt;I have a problem with processor expert and generated code.&lt;/P&gt;&lt;P&gt;I add the PinSettings component to my project and configured needed pins. In the folder “Generated Code” I can see the file pin_mux with corresponding structures. But I can not find the way, how I can add the automatic initialization function to my main.c file. The same for other components.&lt;/P&gt;&lt;P&gt;The HELP says „&lt;FONT face="Times New Roman, serif"&gt;&lt;FONT size="3"&gt;You can let Processor Expert call the Init method automatically by selecting "yes" for the Call Init method in the Initialization group of the Component's properties. „ &lt;/FONT&gt;&lt;/FONT&gt;&lt;FONT face="Times New Roman, serif"&gt;&lt;FONT size="3"&gt;But there is no such setting by me. &lt;/FONT&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Times New Roman, serif"&gt;&lt;FONT size="3"&gt;Thank you very much for your help!&lt;/FONT&gt;&lt;/FONT&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 08 Oct 2020 13:21:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Processor-Expert-for-S32DS-for-ARM/m-p/1164540#M8425</guid>
      <dc:creator>DenisT1980</dc:creator>
      <dc:date>2020-10-08T13:21:19Z</dc:date>
    </item>
    <item>
      <title>Re: Processor Expert for S32DS for ARM</title>
      <link>https://community.nxp.com/t5/S32K/Processor-Expert-for-S32DS-for-ARM/m-p/1164548#M8426</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;you can initialize the GPIOs with the following code line:&lt;/P&gt;&lt;P&gt;PINS_DRV_Init(NUM_OF_CONFIGURED_PINS, g_pin_mux_InitConfigArr);&lt;/P&gt;&lt;P&gt;Place it in your application where you need to initialize the GPIOs.&lt;/P&gt;&lt;P&gt;Tom&lt;/P&gt;</description>
      <pubDate>Thu, 08 Oct 2020 13:37:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Processor-Expert-for-S32DS-for-ARM/m-p/1164548#M8426</guid>
      <dc:creator>TomLightning</dc:creator>
      <dc:date>2020-10-08T13:37:39Z</dc:date>
    </item>
    <item>
      <title>Re: Processor Expert for S32DS for ARM</title>
      <link>https://community.nxp.com/t5/S32K/Processor-Expert-for-S32DS-for-ARM/m-p/1165130#M8435</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Also, I would like to mention if you are not sure how to use some PE components you can look at the available examples located in the S32DS File -&amp;gt; New -&amp;gt; S32DS Project from Example -&amp;gt; S32SDK S32K1xx RTM v 3.0.0 ErxampleProjects&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I hope it helps.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Diana&lt;/P&gt;</description>
      <pubDate>Fri, 09 Oct 2020 11:01:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Processor-Expert-for-S32DS-for-ARM/m-p/1165130#M8435</guid>
      <dc:creator>dianabatrlova</dc:creator>
      <dc:date>2020-10-09T11:01:05Z</dc:date>
    </item>
  </channel>
</rss>