<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: About low power / sleep problems in S32K</title>
    <link>https://community.nxp.com/t5/S32K/About-low-power-sleep-problems/m-p/676275#M841</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Daniel:&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;I have a 33 ohm precision resistor at the MCU power supply terminal. I confirm the current on the basis of the voltage across the resistor to determine the power consumption of the MCU. When the SIRC is switched to 2M, the current is about 10mA in the VPLR mode, but the power consumption in the VPLS mode is almost the same as that in the RUN mode.&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;Also, I changed the SIRC, I run my other programs will run to fly, I did not change the SIRC before, there are also running when flying, such as SPI, baud rate is 500K, CAN 500K,and then open PIT, timed 1ms. Later, I changed the SPI baud rate to 1M is ok.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/19937i4D84983D50746C27/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;This time, I changed the SIRC to 2M, the program opens SYSTICK 1ms, SPI, CAN, the program runs as long as a fly, the probability is 100%, but I changed to 8M on all right.It's like a chip bug, and I'm worried about the chip right now.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 13 Jun 2017 01:25:44 GMT</pubDate>
    <dc:creator>eautopower</dc:creator>
    <dc:date>2017-06-13T01:25:44Z</dc:date>
    <item>
      <title>About low power / sleep problems</title>
      <link>https://community.nxp.com/t5/S32K/About-low-power-sleep-problems/m-p/676265#M831</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi:&lt;/P&gt;&lt;P&gt;S32DS gives an example of power management. If MCU goes into sleep, what external interrupts can wake it up? How do you wake up?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;best wish&lt;/P&gt;&lt;P&gt;xie&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Jun 2017 06:24:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/About-low-power-sleep-problems/m-p/676265#M831</guid>
      <dc:creator>eautopower</dc:creator>
      <dc:date>2017-06-06T06:24:08Z</dc:date>
    </item>
    <item>
      <title>Re: About low power / sleep problems</title>
      <link>https://community.nxp.com/t5/S32K/About-low-power-sleep-problems/m-p/676266#M832</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;All available wake-up sources are listed in Table 7.3.1 of the RM.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Jun 2017 10:57:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/About-low-power-sleep-problems/m-p/676266#M832</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2017-06-06T10:57:15Z</dc:date>
    </item>
    <item>
      <title>Re: About low power / sleep problems</title>
      <link>https://community.nxp.com/t5/S32K/About-low-power-sleep-problems/m-p/676267#M833</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Daniel：&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;I use the power management example in S32DS. I can only switch between HSRUN and RUN mode. I can't enter VLPR or VLPS mode. Why?I&amp;nbsp;switched &amp;nbsp;from module to logical diagram in datasheet,How can I to do if I want to enter VLPR and VLPS?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Jun 2017 05:05:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/About-low-power-sleep-problems/m-p/676267#M833</guid>
      <dc:creator>eautopower</dc:creator>
      <dc:date>2017-06-07T05:05:44Z</dc:date>
    </item>
    <item>
      <title>Re: About low power / sleep problems</title>
      <link>https://community.nxp.com/t5/S32K/About-low-power-sleep-problems/m-p/676268#M834</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;LVPS and VLPR modes cannot be entered from HSRUN mode but only from RUN mode. I would recommend to simplify the example code and use the &lt;SPAN style="color: black;"&gt;POWER_SYS_SetMode&lt;/SPAN&gt; function directly without UART in debug mode.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Jun 2017 13:15:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/About-low-power-sleep-problems/m-p/676268#M834</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2017-06-07T13:15:30Z</dc:date>
    </item>
    <item>
      <title>Re: About low power / sleep problems</title>
      <link>https://community.nxp.com/t5/S32K/About-low-power-sleep-problems/m-p/676269#M835</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;That's what I did，I also switched from RUN mode to VLPR/VLPS, but not into VLPR/VLPS mode,like this:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/20026i27C759BD49FB57EF/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_3.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/20107iBCEFAAD06AC04784/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Jun 2017 01:10:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/About-low-power-sleep-problems/m-p/676269#M835</guid>
      <dc:creator>eautopower</dc:creator>
      <dc:date>2017-06-08T01:10:37Z</dc:date>
    </item>
    <item>
      <title>Re: About low power / sleep problems</title>
      <link>https://community.nxp.com/t5/S32K/About-low-power-sleep-problems/m-p/676270#M836</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have checked the SDK example. I can enter every mode except for VLPR. A hard fault is triggered on an attempt to enter this mode.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;There seems to be a problem with a peripheral clock for UART which is set at 8MHz by default. In VLPR mode all peripheral clock must be configured to 4MHz or less. But even though I change SIRCDIV2 to 4MHz, it doesn’t help. &amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I’m able to enter this VLPR mode only when SIRC frequency range is changed to 2MHz.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="SIRC_2MHz.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/20961i6ECBFE8113311909/image-size/large?v=v2&amp;amp;px=999" role="button" title="SIRC_2MHz.png" alt="SIRC_2MHz.png" /&gt;&lt;/span&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I will check with designers.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Jun 2017 20:59:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/About-low-power-sleep-problems/m-p/676270#M836</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2017-06-08T20:59:31Z</dc:date>
    </item>
    <item>
      <title>Re: About low power / sleep problems</title>
      <link>https://community.nxp.com/t5/S32K/About-low-power-sleep-problems/m-p/676271#M837</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Daniel:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/20231iD90CF49155339831/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Debugger can't go in when it run this program,Now mode is&amp;nbsp;STAT_VLPR,Do you have following&amp;nbsp;source code&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_3.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/20495i86CD40754BCC724B/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Jun 2017 09:20:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/About-low-power-sleep-problems/m-p/676271#M837</guid>
      <dc:creator>eautopower</dc:creator>
      <dc:date>2017-06-12T09:20:17Z</dc:date>
    </item>
    <item>
      <title>Re: About low power / sleep problems</title>
      <link>https://community.nxp.com/t5/S32K/About-low-power-sleep-problems/m-p/676272#M838</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;STRONG class="" style="color: #646464; background-color: #ffffff; border: 0px; font-weight: 200; font-size: 1.286rem; padding: 0px 0px 0px 30px;"&gt;&lt;SPAN class="" style="border: 0px; font-weight: inherit; font-size: 18.004px;"&gt;Daniel:&lt;/SPAN&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG class="" style="color: #646464; background-color: #ffffff; border: 0px; font-weight: 200; font-size: 1.286rem; padding: 0px 0px 0px 30px;"&gt;&lt;SPAN class="" style="border: 0px; font-weight: inherit; font-size: 18.004px;"&gt;&amp;nbsp; yes,Now ,it can enter VLPR,But if that's changed. The VLPS model seems to be having problems.&lt;/SPAN&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Jun 2017 09:24:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/About-low-power-sleep-problems/m-p/676272#M838</guid>
      <dc:creator>eautopower</dc:creator>
      <dc:date>2017-06-12T09:24:40Z</dc:date>
    </item>
    <item>
      <title>Re: About low power / sleep problems</title>
      <link>https://community.nxp.com/t5/S32K/About-low-power-sleep-problems/m-p/676273#M839</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;The application note AN5425 Power Management for S32K14x doesn’t contain any additional software.&lt;/P&gt;&lt;P&gt;But all the functions are described. You only need to disable all clock monitors in SCG module and set all clock frequencies so that they meet requirements for VLPR mode. Core, System and Bus clock frequecy must be max 4 MHz and flash clock max 1MHz. Also, all peripheral clock frequencies must be equal or less than 4MHz.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Jun 2017 19:34:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/About-low-power-sleep-problems/m-p/676273#M839</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2017-06-12T19:34:50Z</dc:date>
    </item>
    <item>
      <title>Re: About low power / sleep problems</title>
      <link>https://community.nxp.com/t5/S32K/About-low-power-sleep-problems/m-p/676274#M840</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;What problems do you have with VLPS? &amp;nbsp;I have noticed from the code you attached that you enter VLPS or STOP mode and then you are trying to get frequency. But when the MCU is in stop mode, the debugger is disconnected from the MCU. Also, at the time the CLOCK_SYS_GetFreq function is being executed, the MCU is already awake and the function will return RUN mode frequency. &amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Jun 2017 19:36:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/About-low-power-sleep-problems/m-p/676274#M840</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2017-06-12T19:36:39Z</dc:date>
    </item>
    <item>
      <title>Re: About low power / sleep problems</title>
      <link>https://community.nxp.com/t5/S32K/About-low-power-sleep-problems/m-p/676275#M841</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Daniel:&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;I have a 33 ohm precision resistor at the MCU power supply terminal. I confirm the current on the basis of the voltage across the resistor to determine the power consumption of the MCU. When the SIRC is switched to 2M, the current is about 10mA in the VPLR mode, but the power consumption in the VPLS mode is almost the same as that in the RUN mode.&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;Also, I changed the SIRC, I run my other programs will run to fly, I did not change the SIRC before, there are also running when flying, such as SPI, baud rate is 500K, CAN 500K,and then open PIT, timed 1ms. Later, I changed the SPI baud rate to 1M is ok.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/19937i4D84983D50746C27/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;This time, I changed the SIRC to 2M, the program opens SYSTICK 1ms, SPI, CAN, the program runs as long as a fly, the probability is 100%, but I changed to 8M on all right.It's like a chip bug, and I'm worried about the chip right now.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Jun 2017 01:25:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/About-low-power-sleep-problems/m-p/676275#M841</guid>
      <dc:creator>eautopower</dc:creator>
      <dc:date>2017-06-13T01:25:44Z</dc:date>
    </item>
    <item>
      <title>Re: About low power / sleep problems</title>
      <link>https://community.nxp.com/t5/S32K/About-low-power-sleep-problems/m-p/676276#M842</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I’m not sure if I understand. You were unable to enter VLPR, then you changed SIRC range to 2M and it helped. So you are able to enter the VLPR mode now but some peripherals don’t work, right?&lt;/P&gt;&lt;P&gt;The change of SIRC range also changes SIRCDIV1, SIRCDIV2 frequency for all the peripherals that use these clocks.&lt;/P&gt;&lt;P&gt;Are you sure the MCU is in VLPS mode when the current you measure is almost the same as the current in RUN mode?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P style="border: none; padding: 0in;"&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Jun 2017 12:46:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/About-low-power-sleep-problems/m-p/676276#M842</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2017-06-13T12:46:00Z</dc:date>
    </item>
    <item>
      <title>Re: About low power / sleep problems</title>
      <link>https://community.nxp.com/t5/S32K/About-low-power-sleep-problems/m-p/676277#M843</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi:&lt;/P&gt;&lt;P&gt;I mean SIRC change to 2M, peripherals can not work under the RUN mode, if we only test whether it can into &amp;nbsp;VLPR mode, current consumption is about 10mA, power consumption is reduced a lot, but it doesn't mean much, because I am in the RUN mode, other peripherals are unable to work, as long as other peripherals, program run fly,it will run to the following picture position:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/20179i940AF85F9F7846FB/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;What we need is how to get MCU into sleep, the current after sleep, as Datasheet explains.and in RUN/HSRUN mode, the program doesn't run fly.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Jun 2017 04:08:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/About-low-power-sleep-problems/m-p/676277#M843</guid>
      <dc:creator>eautopower</dc:creator>
      <dc:date>2017-06-14T04:08:35Z</dc:date>
    </item>
    <item>
      <title>Re: About low power / sleep problems</title>
      <link>https://community.nxp.com/t5/S32K/About-low-power-sleep-problems/m-p/676278#M844</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Well, the SDK seems to be having some problems because you should be able to enter the VLPR mode while the SIRC range is set to 8MHz. I have already reported the issue. The DefaultISR might be a hardfault due to some overclocking.&lt;/P&gt;&lt;P&gt;I would recommend to leave the SIRC range at 8MHz and use the code which is described in the AN5425 Power Management for S32K14x to enter the VLPR/VLPS modes. &lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Jun 2017 13:15:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/About-low-power-sleep-problems/m-p/676278#M844</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2017-06-14T13:15:32Z</dc:date>
    </item>
    <item>
      <title>Re: About low power / sleep problems</title>
      <link>https://community.nxp.com/t5/S32K/About-low-power-sleep-problems/m-p/676279#M845</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;Hi Daniel:&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;&amp;nbsp;What's the progress regarding power management?Do all IO interrupts interrupt sleep?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Jun 2017 06:48:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/About-low-power-sleep-problems/m-p/676279#M845</guid>
      <dc:creator>eautopower</dc:creator>
      <dc:date>2017-06-20T06:48:15Z</dc:date>
    </item>
    <item>
      <title>Re: About low power / sleep problems</title>
      <link>https://community.nxp.com/t5/S32K/About-low-power-sleep-problems/m-p/676280#M846</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Sorry for the delay.&lt;/P&gt;&lt;P&gt;I have received a response from the SDK team. They still investigate the issue.&lt;/P&gt;&lt;P&gt;Wake-up sources are listed in Table 7.3.1 in RM. Pin interrupts are configurable in Port module (PORT_PCRn), during a stop mode they also generates a wake-up signal to exit low-power modes.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 Jun 2017 08:06:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/About-low-power-sleep-problems/m-p/676280#M846</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2017-06-26T08:06:58Z</dc:date>
    </item>
    <item>
      <title>Re: About low power / sleep problems</title>
      <link>https://community.nxp.com/t5/S32K/About-low-power-sleep-problems/m-p/676281#M847</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The SDK team have found the cause of the VLPR issue.&lt;/P&gt;&lt;P&gt;It is caused by a bug in a clock manager component.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To fix it, in the PowerManager example project in &lt;STRONG&gt;DSK/platform/hal/scr/scg/scg_hal.c&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;change &lt;STRONG&gt;regAddr = &amp;amp;base-&amp;gt;VCCR&lt;/STRONG&gt; &amp;nbsp;to &lt;STRONG&gt;regAddr = &amp;amp;base-&amp;gt;HCCR (line 186)&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;remove line 187 with &lt;STRONG&gt;base-&amp;gt;HCCR = value&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="sdk_bug_fix.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/24499iB2D82BF98AE14973/image-size/large?v=v2&amp;amp;px=999" role="button" title="sdk_bug_fix.png" alt="sdk_bug_fix.png" /&gt;&lt;/span&gt;&amp;nbsp;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This bug will be fixed in the release after RTM SDK (0.8.3).&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Jun 2017 10:40:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/About-low-power-sleep-problems/m-p/676281#M847</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2017-06-29T10:40:50Z</dc:date>
    </item>
  </channel>
</rss>