<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic write in D-Flash (or P-flash) with IAP? (in application programming) in S32K</title>
    <link>https://community.nxp.com/t5/S32K/write-in-D-Flash-or-P-flash-with-IAP-in-application-programming/m-p/1161323#M8355</link>
    <description>&lt;P&gt;Hi.&lt;/P&gt;&lt;P&gt;in S32K14x series, there is flash module with 2 bank: P-Flash (Bank 0) and D-Flash (bank 1).&lt;/P&gt;&lt;P&gt;D-Flash can be FlexNVM for whole space or in a partition. assume I want to use FlexNVM with 32 KB from 64KB. so I have EEE with 4KB FlexRAM and back up space with 32 KB space.&lt;/P&gt;&lt;P&gt;the left 32KB partition is D-Flash now. can I write on this space individually ? (not write in FlexRAM &amp;amp; EEE unit).&lt;/P&gt;&lt;P&gt;literally I want to have some EEPROM emulated memory and some D-Flash memory with write access. (these procedures are not performed in same time).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks.&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 30 Sep 2020 12:31:05 GMT</pubDate>
    <dc:creator>Ahmad_bozorgi</dc:creator>
    <dc:date>2020-09-30T12:31:05Z</dc:date>
    <item>
      <title>write in D-Flash (or P-flash) with IAP? (in application programming)</title>
      <link>https://community.nxp.com/t5/S32K/write-in-D-Flash-or-P-flash-with-IAP-in-application-programming/m-p/1161323#M8355</link>
      <description>&lt;P&gt;Hi.&lt;/P&gt;&lt;P&gt;in S32K14x series, there is flash module with 2 bank: P-Flash (Bank 0) and D-Flash (bank 1).&lt;/P&gt;&lt;P&gt;D-Flash can be FlexNVM for whole space or in a partition. assume I want to use FlexNVM with 32 KB from 64KB. so I have EEE with 4KB FlexRAM and back up space with 32 KB space.&lt;/P&gt;&lt;P&gt;the left 32KB partition is D-Flash now. can I write on this space individually ? (not write in FlexRAM &amp;amp; EEE unit).&lt;/P&gt;&lt;P&gt;literally I want to have some EEPROM emulated memory and some D-Flash memory with write access. (these procedures are not performed in same time).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 30 Sep 2020 12:31:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/write-in-D-Flash-or-P-flash-with-IAP-in-application-programming/m-p/1161323#M8355</guid>
      <dc:creator>Ahmad_bozorgi</dc:creator>
      <dc:date>2020-09-30T12:31:05Z</dc:date>
    </item>
    <item>
      <title>Re: write in D-Flash (or P-flash) with IAP? (in application programming)</title>
      <link>https://community.nxp.com/t5/S32K/write-in-D-Flash-or-P-flash-with-IAP-in-application-programming/m-p/1161766#M8368</link>
      <description>&lt;P&gt;Hi Ahmad,&lt;/P&gt;
&lt;P&gt;yes, that's possible. D-Flash which is not allocated for EEE can be used as a normal D-Flash using normal flash commands for program/erase.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 01 Oct 2020 11:13:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/write-in-D-Flash-or-P-flash-with-IAP-in-application-programming/m-p/1161766#M8368</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2020-10-01T11:13:41Z</dc:date>
    </item>
  </channel>
</rss>