<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Flex IO simulate UART in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Flex-IO-simulate-UART/m-p/1155386#M8200</link>
    <description>&lt;P&gt;Hello,I want to use Flex IO to simulate the UART that with even parity function,I read the reference manual and found this statement is the Flex IO module :&lt;/P&gt;&lt;P&gt;&lt;EM&gt;"FlexIO does not support automatic insertion of parity bits." and "FlexIO does not support automatic verification of parity bits."&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;I want to know whether the statement above means that FlexIO doesn't not support the the parity function or FlexIO support the parity function but need to achive it mannually.Can someone tell me about this problem,sincely thanks.&lt;/P&gt;</description>
    <pubDate>Fri, 18 Sep 2020 08:26:30 GMT</pubDate>
    <dc:creator>leo_liu2</dc:creator>
    <dc:date>2020-09-18T08:26:30Z</dc:date>
    <item>
      <title>Flex IO simulate UART</title>
      <link>https://community.nxp.com/t5/S32K/Flex-IO-simulate-UART/m-p/1155386#M8200</link>
      <description>&lt;P&gt;Hello,I want to use Flex IO to simulate the UART that with even parity function,I read the reference manual and found this statement is the Flex IO module :&lt;/P&gt;&lt;P&gt;&lt;EM&gt;"FlexIO does not support automatic insertion of parity bits." and "FlexIO does not support automatic verification of parity bits."&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;I want to know whether the statement above means that FlexIO doesn't not support the the parity function or FlexIO support the parity function but need to achive it mannually.Can someone tell me about this problem,sincely thanks.&lt;/P&gt;</description>
      <pubDate>Fri, 18 Sep 2020 08:26:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Flex-IO-simulate-UART/m-p/1155386#M8200</guid>
      <dc:creator>leo_liu2</dc:creator>
      <dc:date>2020-09-18T08:26:30Z</dc:date>
    </item>
  </channel>
</rss>