<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックControl a Contactor/Relay using S32K144EVB</title>
    <link>https://community.nxp.com/t5/S32K/Control-a-Contactor-Relay-using-S32K144EVB/m-p/1154941#M8186</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have a S32k144EVB and I want to control the contactor using GPIO pins. The contactor already has an internal diode for coil suppression. The coil voltage is 12VDC and coil current is 0.23A.&lt;/P&gt;&lt;P&gt;I could find information of GPIO pullup resistors. Can you please provide this information?&lt;/P&gt;&lt;P&gt;Do I just need to connect external driver, maybe ULN driver or a transistor circuit? Or what is the best way to control a contactor using s32k144evb&lt;/P&gt;&lt;P&gt;Thanks for help&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 17 Sep 2020 16:15:34 GMT</pubDate>
    <dc:creator>rparveez</dc:creator>
    <dc:date>2020-09-17T16:15:34Z</dc:date>
    <item>
      <title>Control a Contactor/Relay using S32K144EVB</title>
      <link>https://community.nxp.com/t5/S32K/Control-a-Contactor-Relay-using-S32K144EVB/m-p/1154941#M8186</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have a S32k144EVB and I want to control the contactor using GPIO pins. The contactor already has an internal diode for coil suppression. The coil voltage is 12VDC and coil current is 0.23A.&lt;/P&gt;&lt;P&gt;I could find information of GPIO pullup resistors. Can you please provide this information?&lt;/P&gt;&lt;P&gt;Do I just need to connect external driver, maybe ULN driver or a transistor circuit? Or what is the best way to control a contactor using s32k144evb&lt;/P&gt;&lt;P&gt;Thanks for help&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 17 Sep 2020 16:15:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Control-a-Contactor-Relay-using-S32K144EVB/m-p/1154941#M8186</guid>
      <dc:creator>rparveez</dc:creator>
      <dc:date>2020-09-17T16:15:34Z</dc:date>
    </item>
    <item>
      <title>Re: Control a Contactor/Relay using S32K144EVB</title>
      <link>https://community.nxp.com/t5/S32K/Control-a-Contactor-Relay-using-S32K144EVB/m-p/1155347#M8197</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;for GPIO pull up value please refer to Table 17 and 18 of the DS;&amp;nbsp;&lt;A href="https://www.nxp.com/docs/en/data-sheet/S32K-DS.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/data-sheet/S32K-DS.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;To control a relay you need to use driver or transistor as you wrote. You can find many suggestions on the web fro this.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Fri, 18 Sep 2020 07:27:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Control-a-Contactor-Relay-using-S32K144EVB/m-p/1155347#M8197</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2020-09-18T07:27:18Z</dc:date>
    </item>
    <item>
      <title>Re: Control a Contactor/Relay using S32K144EVB</title>
      <link>https://community.nxp.com/t5/S32K/Control-a-Contactor-Relay-using-S32K144EVB/m-p/1160697#M8335</link>
      <description>&lt;P&gt;Hi PetrS,&lt;/P&gt;&lt;P&gt;I used PTE14 J05-06 Pin for contactor control with simple model where I just switched 0-5V every 30s with Green LED switching whenever there is voltage change at the pin. I used ULN driver to drive the contactor. This was working fine but all of sudden the S32K144 stopped working and only D2 is blinking. It does not work even if I try to download any other example model (from MBDT lib in Mathworks).&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can you please let me know if its because I toasted something on board?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Rubeena&lt;/P&gt;</description>
      <pubDate>Tue, 29 Sep 2020 12:51:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Control-a-Contactor-Relay-using-S32K144EVB/m-p/1160697#M8335</guid>
      <dc:creator>rparveez</dc:creator>
      <dc:date>2020-09-29T12:51:54Z</dc:date>
    </item>
  </channel>
</rss>