<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32K144_FlexCAN in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K144-FlexCAN/m-p/1153461#M8163</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;assuming the 40Mhz PE clock the setting looks correct.&lt;/P&gt;
&lt;P&gt;For different PE clock you can try to use below excel tool for possible setting.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/MPC5xxx-S32Kxx-CAN-CAN-FD-bit-timing-calculation/ta-p/1119319" target="_blank"&gt;https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/MPC5xxx-S32Kxx-CAN-CAN-FD-bit-timing-calculation/ta-p/1119319&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR, Petr&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 15 Sep 2020 11:36:40 GMT</pubDate>
    <dc:creator>PetrS</dc:creator>
    <dc:date>2020-09-15T11:36:40Z</dc:date>
    <item>
      <title>S32K144_FlexCAN</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-FlexCAN/m-p/1153409#M8159</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'am using the example "FLEXCAN" for the s32k144 board. For my purpose, I want to have as baud rate 50KSamples/second. From the theory I understood that, it is important to modify some fields of CTRL register for the desired baud rate. So, I want to know if it's correct this configuration for the baud rate equal to 50KSamples/seconds.&lt;BR /&gt;&lt;BR /&gt;CAN_CTRL1_PRESDIV(49) (40MHz/(49+1)) = 800KHz&lt;BR /&gt;CAN_CTRL1_PSEG2(3) /* Configure for 50 KHz bit time */&lt;BR /&gt;CAN_CTRL1_PSEG1(3) /* Time quanta freq = 16 time quanta x 50 KHz bit time= 800KHz */&lt;BR /&gt;CAN_CTRL1_PROPSEG(6) /* PRESDIV+1 = Fclksrc/Ftq = 8 MHz/8 MHz = 1 */&lt;BR /&gt;CAN_CTRL1_RJW(3) /* so PRESDIV = 0 */&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;Is this configuration correct for the baud rate equal to 50Ksamples/second?&lt;BR /&gt;In addition, how it is possible to modify the clock requirements for the slow run mode and so for the bus clock equal to 48MHz?&lt;BR /&gt;Thanks for your help&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Paola&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 15 Sep 2020 10:00:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-FlexCAN/m-p/1153409#M8159</guid>
      <dc:creator>p_decesare</dc:creator>
      <dc:date>2020-09-15T10:00:30Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144_FlexCAN</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-FlexCAN/m-p/1153461#M8163</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;assuming the 40Mhz PE clock the setting looks correct.&lt;/P&gt;
&lt;P&gt;For different PE clock you can try to use below excel tool for possible setting.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/MPC5xxx-S32Kxx-CAN-CAN-FD-bit-timing-calculation/ta-p/1119319" target="_blank"&gt;https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/MPC5xxx-S32Kxx-CAN-CAN-FD-bit-timing-calculation/ta-p/1119319&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR, Petr&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 15 Sep 2020 11:36:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-FlexCAN/m-p/1153461#M8163</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2020-09-15T11:36:40Z</dc:date>
    </item>
  </channel>
</rss>