<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: I2C in S32K</title>
    <link>https://community.nxp.com/t5/S32K/I2C/m-p/1152897#M8142</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;1. The Timing Parameters are explained in the RM rev.12.1 Section 52.3.2.4.&lt;/P&gt;
&lt;P&gt;SCL/SDA_RISETIME is given by the resistance of the pull-ups and the capacitance of the bus.&lt;/P&gt;
&lt;P&gt;So you can adjust the parameters (make sure it follows the Table 52-8. LPI2C Timing Parameter Restrictions) or use stronger pull-ups.&lt;/P&gt;
&lt;P&gt;2. Yes, the HIGH period of the SCL clock depends on the SCL_LATENCY as well.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;</description>
    <pubDate>Mon, 14 Sep 2020 12:18:37 GMT</pubDate>
    <dc:creator>danielmartynek</dc:creator>
    <dc:date>2020-09-14T12:18:37Z</dc:date>
    <item>
      <title>I2C</title>
      <link>https://community.nxp.com/t5/S32K/I2C/m-p/1152076#M8132</link>
      <description>&lt;P&gt;hi everyone：&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I find when i use S32K146 to communicate with slave，the I2C frequency will reduction if i connect more than 5 slaves. My question is :&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;SPAN&gt;1&lt;/SPAN&gt;、&lt;SPAN&gt;Is there a quantitative formula for the relationship between load and frequency&lt;/SPAN&gt;？&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 2&lt;/SPAN&gt;、&lt;SPAN&gt;The rising edge time exceeds which critical value will affect my minimum high level time&lt;/SPAN&gt;&lt;SPAN&gt;？&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 11 Sep 2020 09:33:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/I2C/m-p/1152076#M8132</guid>
      <dc:creator>jianminyang</dc:creator>
      <dc:date>2020-09-11T09:33:01Z</dc:date>
    </item>
    <item>
      <title>Re: I2C</title>
      <link>https://community.nxp.com/t5/S32K/I2C/m-p/1152897#M8142</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;1. The Timing Parameters are explained in the RM rev.12.1 Section 52.3.2.4.&lt;/P&gt;
&lt;P&gt;SCL/SDA_RISETIME is given by the resistance of the pull-ups and the capacitance of the bus.&lt;/P&gt;
&lt;P&gt;So you can adjust the parameters (make sure it follows the Table 52-8. LPI2C Timing Parameter Restrictions) or use stronger pull-ups.&lt;/P&gt;
&lt;P&gt;2. Yes, the HIGH period of the SCL clock depends on the SCL_LATENCY as well.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;</description>
      <pubDate>Mon, 14 Sep 2020 12:18:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/I2C/m-p/1152897#M8142</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2020-09-14T12:18:37Z</dc:date>
    </item>
  </channel>
</rss>