<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: S32K1xx:interruption problem</title>
    <link>https://community.nxp.com/t5/S32K/S32K1xx-interruption-problem/m-p/1096011#M8037</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp;Zhibing,&lt;/P&gt;&lt;P&gt;You may need to use the RX FIFO instead of use Message Buffer to achieve it.&lt;BR /&gt;About the RX FIFO, you can refer: &lt;A _jive_internal="true" href="https://community.nxp.com/message/998624"&gt;What is the difference between RX FIFO and message box&lt;/A&gt;&lt;BR /&gt;You can refer this: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-343091"&gt;Example S32K144 FlexCAN RXFIFO DMA S32DS.ARM.2018.R1&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Robin&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Apr 2020 09:00:47 GMT</pubDate>
    <dc:creator>Robin_Shen</dc:creator>
    <dc:date>2020-04-15T09:00:47Z</dc:date>
    <item>
      <title>S32K1xx:interruption problem</title>
      <link>https://community.nxp.com/t5/S32K/S32K1xx-interruption-problem/m-p/1096010#M8036</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi:&lt;/P&gt;&lt;P&gt;status_t FLEXCAN_DRV_ConfigRxMb(uint8_t instance,uint8_t mb_idx,const flexcan_data_info_t *rx_info,uint32_t msg_id)&lt;/P&gt;&lt;P&gt;void FLEXCAN_DRV_InstallEventCallback(uint8_t instance,flexcan_callback_t callback,void *callbackParam)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;if i want to&amp;nbsp;enter interrupt when i receive two or more message,what should set?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your answer！&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Apr 2020 12:43:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K1xx-interruption-problem/m-p/1096010#M8036</guid>
      <dc:creator>shengzhibing</dc:creator>
      <dc:date>2020-04-14T12:43:48Z</dc:date>
    </item>
    <item>
      <title>Re: S32K1xx:interruption problem</title>
      <link>https://community.nxp.com/t5/S32K/S32K1xx-interruption-problem/m-p/1096011#M8037</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp;Zhibing,&lt;/P&gt;&lt;P&gt;You may need to use the RX FIFO instead of use Message Buffer to achieve it.&lt;BR /&gt;About the RX FIFO, you can refer: &lt;A _jive_internal="true" href="https://community.nxp.com/message/998624"&gt;What is the difference between RX FIFO and message box&lt;/A&gt;&lt;BR /&gt;You can refer this: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-343091"&gt;Example S32K144 FlexCAN RXFIFO DMA S32DS.ARM.2018.R1&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Robin&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Apr 2020 09:00:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K1xx-interruption-problem/m-p/1096011#M8037</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2020-04-15T09:00:47Z</dc:date>
    </item>
    <item>
      <title>Re: S32K1xx:interruption problem</title>
      <link>https://community.nxp.com/t5/S32K/S32K1xx-interruption-problem/m-p/1096012#M8038</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Robin_Shen:&lt;/P&gt;&lt;P&gt;Thank you for your reply, which is very useful to me.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Best Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Zhibing Sheng&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Apr 2020 13:03:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K1xx-interruption-problem/m-p/1096012#M8038</guid>
      <dc:creator>shengzhibing</dc:creator>
      <dc:date>2020-04-15T13:03:49Z</dc:date>
    </item>
  </channel>
</rss>