<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32K148 FLEXCAN cannot get IDHIT value in RXFIR or in RX FIFO in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K148-FLEXCAN-cannot-get-IDHIT-value-in-RXFIR-or-in-RX-FIFO/m-p/1087992#M7823</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes the RXFIR includes IDHIT and it is valid&amp;nbsp;while the IFLAG1[BUF5I] flag is asserted. The RXFIR register must&lt;BR /&gt;be read only before clearing the flag. Also IDHIT can be read&amp;nbsp;from C/S word, as shown in the Rx FIFO Structure description.&lt;/P&gt;&lt;P&gt;If have issues still please share filter table, mask registers and the way you read RXFIFO and RXFIR.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 12 Jun 2020 07:11:37 GMT</pubDate>
    <dc:creator>PetrS</dc:creator>
    <dc:date>2020-06-12T07:11:37Z</dc:date>
    <item>
      <title>S32K148 FLEXCAN cannot get IDHIT value in RXFIR or in RX FIFO</title>
      <link>https://community.nxp.com/t5/S32K/S32K148-FLEXCAN-cannot-get-IDHIT-value-in-RXFIR-or-in-RX-FIFO/m-p/1087991#M7822</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The configuration is using RX FIFO and interrupt. I can read a message from the CAN BUS, and I can output a message. I setup 8 ID filters for RX FIFO. The filters work fine - there is no interrupt when there is no ID match, and there IS a RXFIFO interrupt when there is one match. However, regardless where I put the correct ID filter, the RXFIR always shows IDHIT as 0. Should not it show the index of the matching filter?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Jun 2020 23:43:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K148-FLEXCAN-cannot-get-IDHIT-value-in-RXFIR-or-in-RX-FIFO/m-p/1087991#M7822</guid>
      <dc:creator>jlu</dc:creator>
      <dc:date>2020-06-11T23:43:49Z</dc:date>
    </item>
    <item>
      <title>Re: S32K148 FLEXCAN cannot get IDHIT value in RXFIR or in RX FIFO</title>
      <link>https://community.nxp.com/t5/S32K/S32K148-FLEXCAN-cannot-get-IDHIT-value-in-RXFIR-or-in-RX-FIFO/m-p/1087992#M7823</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes the RXFIR includes IDHIT and it is valid&amp;nbsp;while the IFLAG1[BUF5I] flag is asserted. The RXFIR register must&lt;BR /&gt;be read only before clearing the flag. Also IDHIT can be read&amp;nbsp;from C/S word, as shown in the Rx FIFO Structure description.&lt;/P&gt;&lt;P&gt;If have issues still please share filter table, mask registers and the way you read RXFIFO and RXFIR.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Jun 2020 07:11:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K148-FLEXCAN-cannot-get-IDHIT-value-in-RXFIR-or-in-RX-FIFO/m-p/1087992#M7823</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2020-06-12T07:11:37Z</dc:date>
    </item>
  </channel>
</rss>