<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: CAN 1 is not working in S32K</title>
    <link>https://community.nxp.com/t5/S32K/CAN-1-is-not-working/m-p/1087897#M7821</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Petr,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ok thank you very much worked now in NXP evaluation board after following your steps.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best wishes,&lt;/P&gt;&lt;P&gt;Nader&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 02 Jul 2020 11:44:09 GMT</pubDate>
    <dc:creator>naderkhamess</dc:creator>
    <dc:date>2020-07-02T11:44:09Z</dc:date>
    <item>
      <title>CAN 1 is not working</title>
      <link>https://community.nxp.com/t5/S32K/CAN-1-is-not-working/m-p/1087895#M7819</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;problem;we have now a custom hw and i can not send&amp;nbsp;a CAN message&lt;/P&gt;&lt;P&gt;in custom hw : i am trying to run the CAN0 (PTB0, PTB1) and CAN1 (PTA12, PTA13), and connect RX with TX pin and still neither&amp;nbsp; i can not see&amp;nbsp;waveform in the oscilloscope&amp;nbsp;nor a message with CAN-usb.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;in S32K148 evb : CAN0 is working with on board transceiver on pins PTE4, PTE5, however CAN 1 still can not work, even connecting Rx and Tx together.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;could you please give me a hint what to do?&amp;nbsp;&lt;/P&gt;&lt;P&gt;am i missing any hw settings for the pcb?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;my objective is to make either CAN 0 or CAN 1 work run with external CAN transceiver.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i also tried to read ECR and ESR1 registers, but i still can't tell and identify what might be the issue.&amp;nbsp;&lt;/P&gt;&lt;P&gt;i tried also PTA6/PTA7 , and PTA12/PTA13.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best wishes,&lt;/P&gt;&lt;P&gt;Nader Khamess&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;@&lt;A _jive_internal="true" class="" data-content-finding="Community" data-userid="211729" data-username="PetrS" href="https://community.nxp.com/people/PetrS" style="color: #3d9ce7; background-color: #ffffff; border: 0px; font-weight: 200; text-decoration: none; font-size: 1.286rem;"&gt;Petr Stancik&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Jun 2020 14:52:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/CAN-1-is-not-working/m-p/1087895#M7819</guid>
      <dc:creator>naderkhamess</dc:creator>
      <dc:date>2020-06-24T14:52:45Z</dc:date>
    </item>
    <item>
      <title>Re: CAN 1 is not working</title>
      <link>https://community.nxp.com/t5/S32K/CAN-1-is-not-working/m-p/1087896#M7820</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i can recommend below testing...&lt;/P&gt;&lt;P&gt;1. connect TX RX pin together without transceiver and send a message. You should see message repeatedly due to missing ACK. TX error counter is 0x80 and module is in error passive. If you see anything else, you have wrong pin setting&lt;/P&gt;&lt;P&gt;2. connect TX RX pins to transceiver normally and have it unconnected from the bus. Send a message. You should see the same as above. If not transceiver could be disabled or it is not terminated.&lt;/P&gt;&lt;P&gt;3. connect transceiver to the bus with other nodes (e.g. CAN tool), send/receive messages. If any error is detected most probably the CAN bit timing is not right. Be sure all nodes use same bitrate and sample point.&lt;/P&gt;&lt;P&gt;You can use below tool for a calculation&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-342618"&gt;https://community.nxp.com/docs/DOC-342618&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Jun 2020 10:41:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/CAN-1-is-not-working/m-p/1087896#M7820</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2020-06-25T10:41:59Z</dc:date>
    </item>
    <item>
      <title>Re: CAN 1 is not working</title>
      <link>https://community.nxp.com/t5/S32K/CAN-1-is-not-working/m-p/1087897#M7821</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Petr,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ok thank you very much worked now in NXP evaluation board after following your steps.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best wishes,&lt;/P&gt;&lt;P&gt;Nader&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Jul 2020 11:44:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/CAN-1-is-not-working/m-p/1087897#M7821</guid>
      <dc:creator>naderkhamess</dc:creator>
      <dc:date>2020-07-02T11:44:09Z</dc:date>
    </item>
  </channel>
</rss>