<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックFLASH_DRV_ProgramSection</title>
    <link>https://community.nxp.com/t5/S32K/FLASH-DRV-ProgramSection/m-p/1085022#M7749</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hello，&lt;/P&gt;&lt;P&gt;when i set FlexSAM to traditional SRAM and erase all flash memory, SRAM boot and when call the following code, why the address 0x6000 is always 0xFFFFFFFF?&lt;/P&gt;&lt;P&gt;whether is it wrong way to use the function&amp;nbsp;&lt;SPAN&gt;FLASH_DRV_ProgramSection?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I expected 1024 data can be write to flash memory by call function&amp;nbsp;FLASH_DRV_ProgramSection.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;for(i= 0; i&amp;lt; 1024; i++)&lt;BR /&gt; {&lt;BR /&gt; *(uint8_t *)(0x14000000 + i) = sourceBuffer[i % 255];&lt;/P&gt;&lt;P&gt;}&lt;BR /&gt; ret = FLASH_DRV_ProgramSection(&amp;amp;flashSSDConfig, 0x6000, 1024);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;wish your help&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 24 Jul 2020 00:50:18 GMT</pubDate>
    <dc:creator>814420552</dc:creator>
    <dc:date>2020-07-24T00:50:18Z</dc:date>
    <item>
      <title>FLASH_DRV_ProgramSection</title>
      <link>https://community.nxp.com/t5/S32K/FLASH-DRV-ProgramSection/m-p/1085022#M7749</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hello，&lt;/P&gt;&lt;P&gt;when i set FlexSAM to traditional SRAM and erase all flash memory, SRAM boot and when call the following code, why the address 0x6000 is always 0xFFFFFFFF?&lt;/P&gt;&lt;P&gt;whether is it wrong way to use the function&amp;nbsp;&lt;SPAN&gt;FLASH_DRV_ProgramSection?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I expected 1024 data can be write to flash memory by call function&amp;nbsp;FLASH_DRV_ProgramSection.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;for(i= 0; i&amp;lt; 1024; i++)&lt;BR /&gt; {&lt;BR /&gt; *(uint8_t *)(0x14000000 + i) = sourceBuffer[i % 255];&lt;/P&gt;&lt;P&gt;}&lt;BR /&gt; ret = FLASH_DRV_ProgramSection(&amp;amp;flashSSDConfig, 0x6000, 1024);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;wish your help&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Jul 2020 00:50:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/FLASH-DRV-ProgramSection/m-p/1085022#M7749</guid>
      <dc:creator>814420552</dc:creator>
      <dc:date>2020-07-24T00:50:18Z</dc:date>
    </item>
    <item>
      <title>Re: FLASH_DRV_ProgramSection</title>
      <link>https://community.nxp.com/t5/S32K/FLASH-DRV-ProgramSection/m-p/1085023#M7750</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Kui Wu,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt; If you look at the description of this command it explains the previous steps you need to do before calling this command:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/66669i3993061E5AEE87DF/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also, remember that the sector size is 2KB.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;Alexis Andalon&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Jul 2020 21:53:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/FLASH-DRV-ProgramSection/m-p/1085023#M7750</guid>
      <dc:creator>Alexis_A</dc:creator>
      <dc:date>2020-07-24T21:53:20Z</dc:date>
    </item>
  </channel>
</rss>