<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32Kのトピックwhat is mean of  resourceSelectCode in the function FLASH_DRV_ReadResource()</title>
    <link>https://community.nxp.com/t5/S32K/what-is-mean-of-resourceSelectCode-in-the-function-FLASH-DRV/m-p/674026#M771</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;FLASH_DRV_ReadResource(const flash_ssd_config_t * pSSDConfig,&lt;BR /&gt; uint32_t dest,&lt;BR /&gt; uint8_t * pDataArray,&lt;BR /&gt; uint8_t resourceSelectCode)&lt;/P&gt;&lt;P&gt;&amp;nbsp;the function is in s32ds'demo of flash. &amp;nbsp;&lt;/P&gt;&lt;P&gt;I want to &amp;nbsp;read &amp;nbsp;flash data, which function I can &amp;nbsp;use;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 26 Jun 2017 11:50:56 GMT</pubDate>
    <dc:creator>xzw</dc:creator>
    <dc:date>2017-06-26T11:50:56Z</dc:date>
    <item>
      <title>what is mean of  resourceSelectCode in the function FLASH_DRV_ReadResource()</title>
      <link>https://community.nxp.com/t5/S32K/what-is-mean-of-resourceSelectCode-in-the-function-FLASH-DRV/m-p/674026#M771</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;FLASH_DRV_ReadResource(const flash_ssd_config_t * pSSDConfig,&lt;BR /&gt; uint32_t dest,&lt;BR /&gt; uint8_t * pDataArray,&lt;BR /&gt; uint8_t resourceSelectCode)&lt;/P&gt;&lt;P&gt;&amp;nbsp;the function is in s32ds'demo of flash. &amp;nbsp;&lt;/P&gt;&lt;P&gt;I want to &amp;nbsp;read &amp;nbsp;flash data, which function I can &amp;nbsp;use;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 Jun 2017 11:50:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/what-is-mean-of-resourceSelectCode-in-the-function-FLASH-DRV/m-p/674026#M771</guid>
      <dc:creator>xzw</dc:creator>
      <dc:date>2017-06-26T11:50:56Z</dc:date>
    </item>
    <item>
      <title>Re: what is mean of  resourceSelectCode in the function FLASH_DRV_ReadResource()</title>
      <link>https://community.nxp.com/t5/S32K/what-is-mean-of-resourceSelectCode-in-the-function-FLASH-DRV/m-p/674027#M772</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I cannot find the FLASH_DRV_ReadResource() function somehow.&lt;/P&gt;&lt;P&gt;Nevertheless, to read Flash you can simply use a pointer to the address you can read&lt;/P&gt;&lt;P&gt;data = *(unsigned int*)address;&lt;/P&gt;&lt;P&gt;or use DMA or use memcpy function (string.h)&lt;/P&gt;&lt;P&gt;memcpy(&amp;amp;destination, &amp;amp;source, number_of_bytes) &lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Jun 2017 08:05:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/what-is-mean-of-resourceSelectCode-in-the-function-FLASH-DRV/m-p/674027#M772</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2017-06-28T08:05:46Z</dc:date>
    </item>
  </channel>
</rss>