<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic secure MCU in S32K</title>
    <link>https://community.nxp.com/t5/S32K/secure-MCU/m-p/1081761#M7680</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hello,&lt;/P&gt;&lt;P&gt;&amp;lt;1&amp;gt;If CEsc is enabled before the device enters the&amp;nbsp;secured mode, you cannot change the device to an&amp;nbsp;unsecured state through the Erase All Blocks command and the Erase All Blocks unsecure command, right?&lt;BR /&gt;&amp;lt;2&amp;gt; At this time, can I only use the Verify Backdoor Access Key command to change the device to an&amp;nbsp;unsecured state? And if I did not configure the back door key before entering the&amp;nbsp;secured mode, is this device unable to permanently change to the&amp;nbsp;unsecured mode? Is there any other way to change to&amp;nbsp;unsecured mode? And because this debugger is not available when using this command, how can I use this command?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 23 Jun 2020 06:13:02 GMT</pubDate>
    <dc:creator>814420552</dc:creator>
    <dc:date>2020-06-23T06:13:02Z</dc:date>
    <item>
      <title>secure MCU</title>
      <link>https://community.nxp.com/t5/S32K/secure-MCU/m-p/1081761#M7680</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hello,&lt;/P&gt;&lt;P&gt;&amp;lt;1&amp;gt;If CEsc is enabled before the device enters the&amp;nbsp;secured mode, you cannot change the device to an&amp;nbsp;unsecured state through the Erase All Blocks command and the Erase All Blocks unsecure command, right?&lt;BR /&gt;&amp;lt;2&amp;gt; At this time, can I only use the Verify Backdoor Access Key command to change the device to an&amp;nbsp;unsecured state? And if I did not configure the back door key before entering the&amp;nbsp;secured mode, is this device unable to permanently change to the&amp;nbsp;unsecured mode? Is there any other way to change to&amp;nbsp;unsecured mode? And because this debugger is not available when using this command, how can I use this command?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Jun 2020 06:13:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/secure-MCU/m-p/1081761#M7680</guid>
      <dc:creator>814420552</dc:creator>
      <dc:date>2020-06-23T06:13:02Z</dc:date>
    </item>
    <item>
      <title>Re: secure MCU</title>
      <link>https://community.nxp.com/t5/S32K/secure-MCU/m-p/1081762#M7681</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Kui,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. That's correct. If CSE is enabled, it's necessary to run DEBUG_CHAL and DEBUG_AUTH commands to erase keys / reset the CSE back to factory state and then mass erase can be executed. If any key is write protected, you can't do that ever.&lt;/P&gt;&lt;P&gt;2. Yes, Verify Backdoor Access Key command is the only way and yes, there's no way to change it to unsecured state. I already commented here:&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" class="link-titled" href="https://community.nxp.com/thread/535751#comment-1332214" title="https://community.nxp.com/thread/535751#comment-1332214"&gt;https://community.nxp.com/thread/535751#comment-1332214&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Lukas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 Jun 2020 10:15:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/secure-MCU/m-p/1081762#M7681</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2020-06-26T10:15:26Z</dc:date>
    </item>
  </channel>
</rss>