<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Debugger mass erase in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Debugger-mass-erase/m-p/1078662#M7594</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Kui Wu,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The command used by the debugger depends on the debugger you're using, usually, in the Segger debugger first calls a normal to erase all but after detecting if there is secured the MCU&amp;nbsp;there's a message mention this and confirmation if you want to unsecure the device. In this case, the&amp;nbsp;debugger try to unsecure the device first writing to the&amp;nbsp;FSEC[SEC].&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also if check the description from the Erase All Block/Erase All Blocks Unsecure you will notice that in the first one there is the following note:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;The Erase All Blocks command aborts if any flash memory is protected by the FPROT register or FDPROT register or if the FlexRAM region is protected by the FEPROT register&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This isn't the same for the unsecure, this will try to erase all the memory regardless of the protection the memory has.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Alexis Andalon&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 12 Aug 2020 18:44:34 GMT</pubDate>
    <dc:creator>Alexis_A</dc:creator>
    <dc:date>2020-08-12T18:44:34Z</dc:date>
    <item>
      <title>Debugger mass erase</title>
      <link>https://community.nxp.com/t5/S32K/Debugger-mass-erase/m-p/1078661#M7593</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;Debugger call mass erase command , is this command the same with erase all blocks unsecured command, thus erase command =&amp;nbsp;&lt;SPAN&gt;erase all blocks unsecured command?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp; if there is write protection,&amp;nbsp;can&amp;nbsp;erase all blocks unsecured command run ok?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp; thanks in advance!&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Aug 2020 04:03:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Debugger-mass-erase/m-p/1078661#M7593</guid>
      <dc:creator>814420552</dc:creator>
      <dc:date>2020-08-11T04:03:19Z</dc:date>
    </item>
    <item>
      <title>Re: Debugger mass erase</title>
      <link>https://community.nxp.com/t5/S32K/Debugger-mass-erase/m-p/1078662#M7594</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Kui Wu,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The command used by the debugger depends on the debugger you're using, usually, in the Segger debugger first calls a normal to erase all but after detecting if there is secured the MCU&amp;nbsp;there's a message mention this and confirmation if you want to unsecure the device. In this case, the&amp;nbsp;debugger try to unsecure the device first writing to the&amp;nbsp;FSEC[SEC].&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also if check the description from the Erase All Block/Erase All Blocks Unsecure you will notice that in the first one there is the following note:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;The Erase All Blocks command aborts if any flash memory is protected by the FPROT register or FDPROT register or if the FlexRAM region is protected by the FEPROT register&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This isn't the same for the unsecure, this will try to erase all the memory regardless of the protection the memory has.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Alexis Andalon&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Aug 2020 18:44:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Debugger-mass-erase/m-p/1078662#M7594</guid>
      <dc:creator>Alexis_A</dc:creator>
      <dc:date>2020-08-12T18:44:34Z</dc:date>
    </item>
  </channel>
</rss>