<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: S32K146EVB Quick Start Guide</title>
    <link>https://community.nxp.com/t5/S32K/S32K146EVB-Quick-Start-Guide/m-p/1077562#M7569</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It works properly&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 23 Jul 2020 21:08:54 GMT</pubDate>
    <dc:creator>thomas_leborgne</dc:creator>
    <dc:date>2020-07-23T21:08:54Z</dc:date>
    <item>
      <title>S32K146EVB Quick Start Guide</title>
      <link>https://community.nxp.com/t5/S32K/S32K146EVB-Quick-Start-Guide/m-p/1077560#M7567</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, I have some difficulty with the board S32K146EVB when I try to connect it to FreeMASTER like the quick start guide.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I follow the step of the qsg (&lt;A href="https://www.nxp.com/document/guide/Get-Started-with-the-S32K146EVB:NGS-S32K146EVB#title1.3"&gt;https://www.nxp.com/document/guide/Get-Started-with-the-S32K146EVB:NGS-S32K146EVB#title1.3&lt;/A&gt;)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Step 1: Power up the Board –EVB Power Supplies&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The jumpers are in position 2-3.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;When I connect the board to the computer the LEDs D2 and D3 are green and the RGB LED blink red or green (depend on the potentiometer) and I see the board as a device storage on the computer&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Step 2: Jumpstart based on the FreeMASTER tool&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My problem appears here.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;When I try to setup the communication (p°14 of the pdf), I cannot choose the port "&lt;EM&gt;opensda&lt;/EM&gt;", I can only choose &lt;EM&gt;COM3&lt;/EM&gt; or &lt;EM&gt;COM_ALL&lt;/EM&gt;. If I select one of them nothing changes.&lt;/P&gt;&lt;P&gt;I try to use the tool Connection Wizard and I have the same problem. I can only choose "&lt;EM&gt;COM3 - OpenSDA - CDC Serial Port&lt;/EM&gt;". When I select it, I have the error "&lt;STRONG&gt;No board detected on any specified UART communication ports&lt;/STRONG&gt;" (I try with all values of the baud-rates).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I find another thread with the same problem (&lt;A _jive_internal="true" href="https://community.nxp.com/thread/504002"&gt;https://community.nxp.com/thread/504002&lt;/A&gt;). I try the solution (open a project on S32 studio, generate the srec file and drag and drop it to the board).&lt;/P&gt;&lt;P&gt;I didn't find the project S32K146 EVB JumpStart - Firmware (Rev 1) so I try with the project find here (&lt;A href="https://www.nxp.com/document/guide/Get-Started-with-the-S32K146EVB:NGS-S32K146EVB#title2.2"&gt;https://www.nxp.com/document/guide/Get-Started-with-the-S32K146EVB:NGS-S32K146EVB#title2.2&lt;/A&gt;). The name of project is "&lt;EM&gt;S32K146_EVB_Hello&lt;/EM&gt;".&lt;/P&gt;&lt;P&gt;I follow this document to create the srec file (&lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-340965"&gt;https://community.nxp.com/docs/DOC-340965&lt;/A&gt;)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;When I put the srec file on the board, the RGB stop to blink, but I still have the same error when I try to use the Connection Wizard.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I also try to find the file "&lt;EM&gt;S32K146EVB_OOBE_FreeMASTER_Firmware.srec&lt;/EM&gt;" but I didn't find it in the design resources of the board.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Jul 2020 10:40:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K146EVB-Quick-Start-Guide/m-p/1077560#M7567</guid>
      <dc:creator>thomas_leborgne</dc:creator>
      <dc:date>2020-07-22T10:40:07Z</dc:date>
    </item>
    <item>
      <title>Re: S32K146EVB Quick Start Guide</title>
      <link>https://community.nxp.com/t5/S32K/S32K146EVB-Quick-Start-Guide/m-p/1077561#M7568</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp;thomas leborgne,&lt;/P&gt;&lt;P&gt;Sorry for the inconvenience we bring you!&lt;BR /&gt;Please download the attached &lt;STRONG&gt;S32K146EVB_OOBE_FreeMASTER_Firmware.srec&lt;/STRONG&gt;&lt;BR /&gt;Then you should be able to connect the board with FreeMASTER.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/116631i4B3DEB2D7A7902E2/image-size/large?v=v2&amp;amp;px=999" title="detected.png" alt="detected.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/116632iE81E2152C9A171B6/image-size/large?v=v2&amp;amp;px=999" title="S32K146EVB_OOBE.png" alt="S32K146EVB_OOBE.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Robin&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Jul 2020 01:19:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K146EVB-Quick-Start-Guide/m-p/1077561#M7568</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2020-07-23T01:19:48Z</dc:date>
    </item>
    <item>
      <title>Re: S32K146EVB Quick Start Guide</title>
      <link>https://community.nxp.com/t5/S32K/S32K146EVB-Quick-Start-Guide/m-p/1077562#M7569</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It works properly&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Jul 2020 21:08:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K146EVB-Quick-Start-Guide/m-p/1077562#M7569</guid>
      <dc:creator>thomas_leborgne</dc:creator>
      <dc:date>2020-07-23T21:08:54Z</dc:date>
    </item>
    <item>
      <title>Re: S32K146EVB Quick Start Guide</title>
      <link>https://community.nxp.com/t5/S32K/S32K146EVB-Quick-Start-Guide/m-p/1211818#M9599</link>
      <description>&lt;P&gt;Hello I am having the same problem, incorrect documentation. After reading conflicting information concerning this same problem, I dragged and dropped the above file when I was in bootloader mode. Now, not only does it still not work, I am stuck in bootloader mode, I cannot get back to application mode.&lt;/P&gt;&lt;P&gt;What is the recovery procedure from this and is there proper, up to date documentation as this problem apparently been around a couple of years.&lt;/P&gt;</description>
      <pubDate>Thu, 14 Jan 2021 15:18:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K146EVB-Quick-Start-Guide/m-p/1211818#M9599</guid>
      <dc:creator>jgraham954</dc:creator>
      <dc:date>2021-01-14T15:18:47Z</dc:date>
    </item>
  </channel>
</rss>