<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: Format SREC</title>
    <link>https://community.nxp.com/t5/S32K/Format-SREC/m-p/1077212#M7560</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It is up to you if you use SREC or other file formats. A bin or hex file can also be used.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Diana&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 09 Jul 2020 08:21:54 GMT</pubDate>
    <dc:creator>dianabatrlova</dc:creator>
    <dc:date>2020-07-09T08:21:54Z</dc:date>
    <item>
      <title>Format SREC</title>
      <link>https://community.nxp.com/t5/S32K/Format-SREC/m-p/1077211#M7559</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;In the bootloader application, why we choose the SREC format to send data.&lt;BR /&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Jul 2020 12:47:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Format-SREC/m-p/1077211#M7559</guid>
      <dc:creator>abderrahimjamao</dc:creator>
      <dc:date>2020-07-08T12:47:51Z</dc:date>
    </item>
    <item>
      <title>Re: Format SREC</title>
      <link>https://community.nxp.com/t5/S32K/Format-SREC/m-p/1077212#M7560</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It is up to you if you use SREC or other file formats. A bin or hex file can also be used.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Diana&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Jul 2020 08:21:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Format-SREC/m-p/1077212#M7560</guid>
      <dc:creator>dianabatrlova</dc:creator>
      <dc:date>2020-07-09T08:21:54Z</dc:date>
    </item>
    <item>
      <title>Re: Format SREC</title>
      <link>https://community.nxp.com/t5/S32K/Format-SREC/m-p/1077213#M7561</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to add a note.&amp;nbsp;&lt;/P&gt;&lt;P&gt;If you are building your own bootloader you can choose the file which you want.&lt;/P&gt;&lt;P&gt;However, our example such as AN12218 is programmed to process SREC. So, if you want to use another format you should change the code.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Diana&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Jul 2020 06:39:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Format-SREC/m-p/1077213#M7561</guid>
      <dc:creator>dianabatrlova</dc:creator>
      <dc:date>2020-07-10T06:39:34Z</dc:date>
    </item>
  </channel>
</rss>