<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: How to put bootloader in D-flash, meanwhile in booloader configure eeprom?</title>
    <link>https://community.nxp.com/t5/S32K/How-to-put-bootloader-in-D-flash-meanwhile-in-booloader/m-p/1073292#M7411</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can&amp;nbsp;configure partitioning right from the PE Micro debugger in debug configuration. However, it may vary for other programmers/debuggers.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/116580i97C9A436E5E0DD81/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Or you can use another project which does the partitioning and after that use the &lt;EM&gt;Preserve Partitioning for the device&lt;/EM&gt; option in your bootloader project.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, I would like to mention that the partitioning should only be done once during the application lifetime.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I hope it helps.&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Diana&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 22 Jul 2020 12:52:46 GMT</pubDate>
    <dc:creator>dianabatrlova</dc:creator>
    <dc:date>2020-07-22T12:52:46Z</dc:date>
    <item>
      <title>How to put bootloader in D-flash, meanwhile in booloader configure eeprom?</title>
      <link>https://community.nxp.com/t5/S32K/How-to-put-bootloader-in-D-flash-meanwhile-in-booloader/m-p/1073291#M7410</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi @all experts,&lt;/P&gt;&lt;P&gt;I have a question, please do me a favor.&lt;/P&gt;&lt;P&gt;I want to put my &lt;STRONG&gt;Bootloader&lt;/STRONG&gt; code in D-flash(starting adress is 0x1000 0000),&amp;nbsp;&lt;STRONG&gt;Application&lt;/STRONG&gt; code in P-flash(starting adress is 0x0000 1000) as in&amp;nbsp;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/application-note/AN12218.pdf" title="https://www.nxp.com/docs/en/application-note/AN12218.pdf"&gt;https://www.nxp.com/docs/en/application-note/AN12218.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_6.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/116539i48D4FA8DD440A44D/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_6.png" alt="pastedImage_6.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Bootloader's liner file, my MCU is S32k142.&lt;/P&gt;&lt;P&gt;&lt;EM&gt;MEMORY&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;{&lt;/EM&gt;&lt;BR /&gt; &lt;EM&gt;/* Flash */&lt;/EM&gt;&lt;BR /&gt; &lt;EM&gt;m_interrupts (RX) : ORIGIN = 0x00000000, LENGTH = 0x00000400&lt;/EM&gt;&lt;BR /&gt; &lt;EM&gt;m_flash_config (RX) : ORIGIN = 0x00000400, LENGTH = 0x00000010&lt;/EM&gt;&lt;BR /&gt; &lt;EM&gt;m_text (RX) : ORIGIN = 0x10000000, LENGTH = 0x00008000&lt;/EM&gt;&lt;BR /&gt; &lt;EM&gt;/* reserve 256-4 = 252KB P-Flash for application*/&lt;/EM&gt;&lt;BR /&gt; &lt;EM&gt;App_flash (RX) : ORIGIN = 0x00001000, LENGTH = 0x0003F000&lt;/EM&gt;&lt;BR /&gt; &lt;EM&gt;/* SRAM_L */&lt;/EM&gt;&lt;BR /&gt; &lt;EM&gt;m_data (RW) : ORIGIN = 0x1FFFC000, LENGTH = 0x00004000&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;/* SRAM_U */&lt;/EM&gt;&lt;BR /&gt; &lt;EM&gt;m_data_2 (RW) : ORIGIN = 0x20000000, LENGTH = 0x00003000&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;}&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; Additionally, I also need eeprom function to record some parameters, so I split the D-flash 32k in BOOTLOADER using&amp;nbsp; FLASH_DRV_DEFlashPartition(&amp;amp;pSSDConfig, 0x02u, 0x0Bu, 0x0u, false, true) in BootLoader. however, when&amp;nbsp; program flow executes the&amp;nbsp;&amp;nbsp;&lt;SPAN&gt;FLASH_DRV_DEFlashPartition(&amp;amp;pSSDConfig, 0x02u, 0x0Bu, 0x0u, false, true) . whole&amp;nbsp;D-flash is erased&amp;nbsp; so&amp;nbsp;&lt;/SPAN&gt;&amp;nbsp;the&amp;nbsp;&lt;EM&gt;m_text (RX) : ORIGIN = 0x10000000, LENGTH = 0x00008000&amp;nbsp; is erased.&amp;nbsp; bootloader is doomed.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/application-note/AN12218.pdf" title="https://www.nxp.com/docs/en/application-note/AN12218.pdf"&gt;https://www.nxp.com/docs/en/application-note/AN12218.pdf&lt;/A&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_8.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/116540i5E46AB56C351EACF/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_8.png" alt="pastedImage_8.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_9.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/116541i23C88EC3E6F4F862/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_9.png" alt="pastedImage_9.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;so I want to ask how to&amp;nbsp;&lt;SPAN&gt;execute the&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;FLASH_DRV_DEFlashPartition(&amp;amp;pSSDConfig, 0x02u, 0x0Bu, 0x0u, false, true)&lt;SPAN&gt;&amp;nbsp; to configure EEPROM without erase bootloader's&amp;nbsp;&amp;nbsp;&lt;EM&gt;m_text (RX) : ORIGIN = 0x10000000, LENGTH = 0x00008000 sector?&lt;/EM&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN&gt;&lt;EM&gt;thanks.&lt;/EM&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN&gt;&lt;EM&gt;@#bootloader&lt;/EM&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Jul 2020 03:35:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/How-to-put-bootloader-in-D-flash-meanwhile-in-booloader/m-p/1073291#M7410</guid>
      <dc:creator>459021854</dc:creator>
      <dc:date>2020-07-22T03:35:53Z</dc:date>
    </item>
    <item>
      <title>Re: How to put bootloader in D-flash, meanwhile in booloader configure eeprom?</title>
      <link>https://community.nxp.com/t5/S32K/How-to-put-bootloader-in-D-flash-meanwhile-in-booloader/m-p/1073292#M7411</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can&amp;nbsp;configure partitioning right from the PE Micro debugger in debug configuration. However, it may vary for other programmers/debuggers.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/116580i97C9A436E5E0DD81/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Or you can use another project which does the partitioning and after that use the &lt;EM&gt;Preserve Partitioning for the device&lt;/EM&gt; option in your bootloader project.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, I would like to mention that the partitioning should only be done once during the application lifetime.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I hope it helps.&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Diana&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Jul 2020 12:52:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/How-to-put-bootloader-in-D-flash-meanwhile-in-booloader/m-p/1073292#M7411</guid>
      <dc:creator>dianabatrlova</dc:creator>
      <dc:date>2020-07-22T12:52:46Z</dc:date>
    </item>
  </channel>
</rss>