<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: About FLEXIO Timer Operation Question in S32K</title>
    <link>https://community.nxp.com/t5/S32K/About-FLEXIO-Timer-Operation-Question/m-p/1069823#M7340</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You have an old version of the S32K reference manual, you can download the newest version available from the following &lt;A href="https://www.nxp.com/webapp/Download?colCode=S32K1XXRM"&gt;link&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now regarding the statement. When the condition configured by timer disable (TIMDIS) is detected, the output of the timer will be cleared, it doesn't matter what is the value of the timer, once this condition is detected this output will be cleared automatically. Clearing the output of the timer won't affect the shifters controlled by this timer, this means that the values won't be shifted when this condition occurs unless you generate a shift event with the timer shift clock.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Victor&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 29 Jul 2020 17:30:43 GMT</pubDate>
    <dc:creator>victorjimenez</dc:creator>
    <dc:date>2020-07-29T17:30:43Z</dc:date>
    <item>
      <title>About FLEXIO Timer Operation Question</title>
      <link>https://community.nxp.com/t5/S32K/About-FLEXIO-Timer-Operation-Question/m-p/1069820#M7337</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN class=""&gt;52.4.3.6 Timer Disable and Stop Bit&lt;/SPAN&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Timer output will clear. Shifters that are controlled by this timer do not see this as a&lt;BR /&gt;falling edge on the timer shift clock, but can generate a shift event if the timer shift&lt;BR /&gt;clock would otherwise generate one&lt;/SPAN&gt; &lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="background-color: #f8f9fa; color: #222222; font-size: 28px; "&gt;This description is incomprehensible, can you elaborate on it&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Jul 2020 09:33:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/About-FLEXIO-Timer-Operation-Question/m-p/1069820#M7337</guid>
      <dc:creator>584914019</dc:creator>
      <dc:date>2020-07-21T09:33:55Z</dc:date>
    </item>
    <item>
      <title>Re: About FLEXIO Timer Operation Question</title>
      <link>https://community.nxp.com/t5/S32K/About-FLEXIO-Timer-Operation-Question/m-p/1069821#M7338</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To provide you better support, could you please specify where exactly did you see that description?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Victor&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Jul 2020 21:12:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/About-FLEXIO-Timer-Operation-Question/m-p/1069821#M7338</guid>
      <dc:creator>victorjimenez</dc:creator>
      <dc:date>2020-07-23T21:12:24Z</dc:date>
    </item>
    <item>
      <title>Re: About FLEXIO Timer Operation Question</title>
      <link>https://community.nxp.com/t5/S32K/About-FLEXIO-Timer-Operation-Question/m-p/1069822#M7339</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;S32K-RM-2019 52.4.3.6 chapter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Jul 2020 10:30:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/About-FLEXIO-Timer-Operation-Question/m-p/1069822#M7339</guid>
      <dc:creator>584914019</dc:creator>
      <dc:date>2020-07-24T10:30:02Z</dc:date>
    </item>
    <item>
      <title>Re: About FLEXIO Timer Operation Question</title>
      <link>https://community.nxp.com/t5/S32K/About-FLEXIO-Timer-Operation-Question/m-p/1069823#M7340</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You have an old version of the S32K reference manual, you can download the newest version available from the following &lt;A href="https://www.nxp.com/webapp/Download?colCode=S32K1XXRM"&gt;link&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now regarding the statement. When the condition configured by timer disable (TIMDIS) is detected, the output of the timer will be cleared, it doesn't matter what is the value of the timer, once this condition is detected this output will be cleared automatically. Clearing the output of the timer won't affect the shifters controlled by this timer, this means that the values won't be shifted when this condition occurs unless you generate a shift event with the timer shift clock.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Victor&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Jul 2020 17:30:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/About-FLEXIO-Timer-Operation-Question/m-p/1069823#M7340</guid>
      <dc:creator>victorjimenez</dc:creator>
      <dc:date>2020-07-29T17:30:43Z</dc:date>
    </item>
  </channel>
</rss>