<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic CAN Current Source Capability in S32K</title>
    <link>https://community.nxp.com/t5/S32K/CAN-Current-Source-Capability/m-p/1067276#M7286</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Currently I'm using S32K14x device. I would like to know the current sink capability of CAN RX Module.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have seen I/O current sinking capability mentioned as 5mA when used as IO pin as shown below. Will it work same with CAN module of any baud rate.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/106909iA6B4D9FECFA89031/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kindly help with suitable documents.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Raju&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 23 May 2020 14:10:20 GMT</pubDate>
    <dc:creator>bjrajendra</dc:creator>
    <dc:date>2020-05-23T14:10:20Z</dc:date>
    <item>
      <title>CAN Current Source Capability</title>
      <link>https://community.nxp.com/t5/S32K/CAN-Current-Source-Capability/m-p/1067276#M7286</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Currently I'm using S32K14x device. I would like to know the current sink capability of CAN RX Module.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have seen I/O current sinking capability mentioned as 5mA when used as IO pin as shown below. Will it work same with CAN module of any baud rate.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/106909iA6B4D9FECFA89031/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kindly help with suitable documents.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Raju&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 23 May 2020 14:10:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/CAN-Current-Source-Capability/m-p/1067276#M7286</guid>
      <dc:creator>bjrajendra</dc:creator>
      <dc:date>2020-05-23T14:10:20Z</dc:date>
    </item>
    <item>
      <title>Re: CAN Current Source Capability</title>
      <link>https://community.nxp.com/t5/S32K/CAN-Current-Source-Capability/m-p/1067277#M7287</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&amp;nbsp;Raju,&lt;/P&gt;&lt;P&gt;The 5mA sink current applies&amp;nbsp;for output pins only.&lt;/P&gt;&lt;P&gt;The CAN_RX function is an input, it is floating.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 May 2020 15:41:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/CAN-Current-Source-Capability/m-p/1067277#M7287</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2020-05-25T15:41:18Z</dc:date>
    </item>
    <item>
      <title>Re: CAN Current Source Capability</title>
      <link>https://community.nxp.com/t5/S32K/CAN-Current-Source-Capability/m-p/1067278#M7288</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Daniel,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the response.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In fact, we're&amp;nbsp;planning to connect two &lt;A href="https://www.nxp.com/docs/en/data-sheet/TJA1050.pdf"&gt;TJA1050&lt;/A&gt;&amp;nbsp;transceiver IC to one CAN_TX &amp;amp; CAN_RX port.&amp;nbsp;This transceiver IC has an RX terminal in the range of 10mA. Thus is it possible for CAN_RX port to deliver the same.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I may be misunderstood. Kindly guide in meeting the requirement.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Raju.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 May 2020 05:15:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/CAN-Current-Source-Capability/m-p/1067278#M7288</guid>
      <dc:creator>bjrajendra</dc:creator>
      <dc:date>2020-05-26T05:15:43Z</dc:date>
    </item>
    <item>
      <title>Re: CAN Current Source Capability</title>
      <link>https://community.nxp.com/t5/S32K/CAN-Current-Source-Capability/m-p/1067279#M7289</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Raju,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The RXD pin of the transceiver is an output, it is not an input.&lt;/P&gt;&lt;P&gt;As you can see below, there is&amp;nbsp;a push-pull driver.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/107764iE85E4C9958178CD8/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Specified as follows:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/107601i31D8A0E401E7E6B7/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The RXD pin of the transceiver is connected to the CAN_RX pin of the MCU.&lt;/P&gt;&lt;P&gt;Where the CAN_RX pin is an input driven by the RXD driver.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/107151i8465900DC202C466/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 May 2020 07:53:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/CAN-Current-Source-Capability/m-p/1067279#M7289</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2020-05-26T07:53:26Z</dc:date>
    </item>
    <item>
      <title>Re: CAN Current Source Capability</title>
      <link>https://community.nxp.com/t5/S32K/CAN-Current-Source-Capability/m-p/1067280#M7290</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Daniel for the support.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Raju.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 May 2020 10:41:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/CAN-Current-Source-Capability/m-p/1067280#M7290</guid>
      <dc:creator>bjrajendra</dc:creator>
      <dc:date>2020-05-26T10:41:34Z</dc:date>
    </item>
  </channel>
</rss>