<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: How to configure half of FlexNVM as D-flash?half of FlexNVM as EEPROM backup region?  in S32K</title>
    <link>https://community.nxp.com/t5/S32K/How-to-configure-half-of-FlexNVM-as-D-flash-half-of-FlexNVM-as/m-p/1066750#M7276</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;it works! thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 22 Jul 2020 01:25:33 GMT</pubDate>
    <dc:creator>459021854</dc:creator>
    <dc:date>2020-07-22T01:25:33Z</dc:date>
    <item>
      <title>How to configure half of FlexNVM as D-flash?half of FlexNVM as EEPROM backup region?</title>
      <link>https://community.nxp.com/t5/S32K/How-to-configure-half-of-FlexNVM-as-D-flash-half-of-FlexNVM-as/m-p/1066747#M7273</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;@&lt;/P&gt;&lt;P&gt;Hi guys,&lt;/P&gt;&lt;P&gt;I have a question, ask for your help.&lt;/P&gt;&lt;P&gt;In the project example of &lt;STRONG&gt;‘flash_partitioning_s32k142’&lt;/STRONG&gt; all of FlexNVM(64k) is set as&amp;nbsp;EEPROM backup region,&amp;nbsp;all of&amp;nbsp;FlexRAM(4K)&amp;nbsp;is set as&amp;nbsp;EEPROM.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/116310i95E29EA049E8B6C2/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could I separate half of&amp;nbsp;FlexNVM as D-flash to store program, and half of&amp;nbsp;&lt;SPAN&gt;FlexNVM&amp;nbsp;as&amp;nbsp;EEPROM backup region?&amp;nbsp;&amp;nbsp;also&amp;nbsp;FlexRAM &amp;nbsp;do not need to be configured as&amp;nbsp;much as 4K to be EEPROM, only need a few bytes needed, Configure rest&amp;nbsp; of FlexRAM as ram?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;If convenient could you give me some reference code.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;‌&lt;A href="https://community.nxp.com/space/11774"&gt;S32 SDK@&lt;/A&gt;all experts&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 Jul 2020 09:09:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/How-to-configure-half-of-FlexNVM-as-D-flash-half-of-FlexNVM-as/m-p/1066747#M7273</guid>
      <dc:creator>459021854</dc:creator>
      <dc:date>2020-07-20T09:09:41Z</dc:date>
    </item>
    <item>
      <title>Re: How to configure half of FlexNVM as D-flash?half of FlexNVM as EEPROM backup region?</title>
      <link>https://community.nxp.com/t5/S32K/How-to-configure-half-of-FlexNVM-as-D-flash-half-of-FlexNVM-as/m-p/1066748#M7274</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;When the partition code is not set to full data flash, the data set size can be set to any of several non-zero values &lt;A href="https://www.dqfansurvey.org/"&gt;dqfansurvey&lt;/A&gt;.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Jul 2020 11:11:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/How-to-configure-half-of-FlexNVM-as-D-flash-half-of-FlexNVM-as/m-p/1066748#M7274</guid>
      <dc:creator>dinarogers1989</dc:creator>
      <dc:date>2020-07-21T11:11:03Z</dc:date>
    </item>
    <item>
      <title>Re: How to configure half of FlexNVM as D-flash?half of FlexNVM as EEPROM backup region?</title>
      <link>https://community.nxp.com/t5/S32K/How-to-configure-half-of-FlexNVM-as-D-flash-half-of-FlexNVM-as/m-p/1066749#M7275</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to suggest checking AN11983 - Using the S32K1xx EEPROM Functionality&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/application-note/AN11983.pdf" title="https://www.nxp.com/docs/en/application-note/AN11983.pdf"&gt;https://www.nxp.com/docs/en/application-note/AN11983.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Yes, it is possible to split FlexNVM.&amp;nbsp;&lt;/P&gt;&lt;P&gt;The options how to split the FlexNVM block between D-Flash and emulated EEPROM backup memory (E-Flash), see below:&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/116445i5D86A0B951732777/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;This setting represents "DEPartitionCode" parameter in the "FLASH_DRV_DEFlashPartition()" function&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;About your second question related to FlexRAM. The FlexRAM cannot be split, we can use only&amp;nbsp;the whole FlexRAM as&amp;nbsp;an SRAM or EEPROM.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope it helps.&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Diana&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Jul 2020 12:01:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/How-to-configure-half-of-FlexNVM-as-D-flash-half-of-FlexNVM-as/m-p/1066749#M7275</guid>
      <dc:creator>dianabatrlova</dc:creator>
      <dc:date>2020-07-21T12:01:50Z</dc:date>
    </item>
    <item>
      <title>Re: How to configure half of FlexNVM as D-flash?half of FlexNVM as EEPROM backup region?</title>
      <link>https://community.nxp.com/t5/S32K/How-to-configure-half-of-FlexNVM-as-D-flash-half-of-FlexNVM-as/m-p/1066750#M7276</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;it works! thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Jul 2020 01:25:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/How-to-configure-half-of-FlexNVM-as-D-flash-half-of-FlexNVM-as/m-p/1066750#M7276</guid>
      <dc:creator>459021854</dc:creator>
      <dc:date>2020-07-22T01:25:33Z</dc:date>
    </item>
  </channel>
</rss>