<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRWW（read while write）</title>
    <link>https://community.nxp.com/t5/S32K/RWW-read-while-write/m-p/1063397#M7192</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hello，&lt;/P&gt;&lt;P&gt;how to test read and write function for S32k146 ?&amp;nbsp; can you give me a demo code for this test?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 25 Aug 2020 03:29:59 GMT</pubDate>
    <dc:creator>814420552</dc:creator>
    <dc:date>2020-08-25T03:29:59Z</dc:date>
    <item>
      <title>RWW（read while write）</title>
      <link>https://community.nxp.com/t5/S32K/RWW-read-while-write/m-p/1063397#M7192</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hello，&lt;/P&gt;&lt;P&gt;how to test read and write function for S32k146 ?&amp;nbsp; can you give me a demo code for this test?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Aug 2020 03:29:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/RWW-read-while-write/m-p/1063397#M7192</guid>
      <dc:creator>814420552</dc:creator>
      <dc:date>2020-08-25T03:29:59Z</dc:date>
    </item>
    <item>
      <title>Re: RWW（read while write）</title>
      <link>https://community.nxp.com/t5/S32K/RWW-read-while-write/m-p/1063398#M7193</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For example, we can see that reading /executing code during an erase/write operation is not allowed on the same flash block in the RM rev 12.1&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/111150iE5892250C5D103FA/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;So, the program phrase functions and erase flash sector functions are a test of "simultaneous flash operations" itself because it cannot run in the same flash block which are being erased/programmed.&lt;/P&gt;&lt;P&gt;For example, in the attached simple test code, you can see these functions which are placed in RAM to avoid executing code/reading from the same flash block during write.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope it helps.&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Diana&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Aug 2020 13:18:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/RWW-read-while-write/m-p/1063398#M7193</guid>
      <dc:creator>dianabatrlova</dc:creator>
      <dc:date>2020-08-26T13:18:02Z</dc:date>
    </item>
  </channel>
</rss>