<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Enable Hysteresis for UART Rx on S32K116 in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Enable-Hysteresis-for-UART-Rx-on-S32K116/m-p/1060254#M7106</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&amp;nbsp;Satheesh,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;These pins can be configured with an internal pull-up, pull-down, or with neither of these two options. You cannot configure different values for the internal pull-up/pull-down resistor.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;/P&gt;&lt;P&gt;Victor&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note:&lt;/P&gt;&lt;P&gt;- If this post answers your question, please click the "Mark Correct"button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;/P&gt;&lt;P&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 22 Jun 2020 20:41:48 GMT</pubDate>
    <dc:creator>victorjimenez</dc:creator>
    <dc:date>2020-06-22T20:41:48Z</dc:date>
    <item>
      <title>Enable Hysteresis for UART Rx on S32K116</title>
      <link>https://community.nxp.com/t5/S32K/Enable-Hysteresis-for-UART-Rx-on-S32K116/m-p/1060253#M7105</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can I configure Hysteresis for UART Rx pin. If yes Can I configure to different values?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Satheesh.&lt;/P&gt;&lt;H1 class="" lang="en"&gt;&lt;/H1&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Jun 2020 15:41:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Enable-Hysteresis-for-UART-Rx-on-S32K116/m-p/1060253#M7105</guid>
      <dc:creator>satheesh_mb</dc:creator>
      <dc:date>2020-06-17T15:41:02Z</dc:date>
    </item>
    <item>
      <title>Re: Enable Hysteresis for UART Rx on S32K116</title>
      <link>https://community.nxp.com/t5/S32K/Enable-Hysteresis-for-UART-Rx-on-S32K116/m-p/1060254#M7106</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&amp;nbsp;Satheesh,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;These pins can be configured with an internal pull-up, pull-down, or with neither of these two options. You cannot configure different values for the internal pull-up/pull-down resistor.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;/P&gt;&lt;P&gt;Victor&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note:&lt;/P&gt;&lt;P&gt;- If this post answers your question, please click the "Mark Correct"button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;/P&gt;&lt;P&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Jun 2020 20:41:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Enable-Hysteresis-for-UART-Rx-on-S32K116/m-p/1060254#M7106</guid>
      <dc:creator>victorjimenez</dc:creator>
      <dc:date>2020-06-22T20:41:48Z</dc:date>
    </item>
  </channel>
</rss>