<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 S32K148 QSPI</title>
    <link>https://community.nxp.com/t5/S32K/S32K148-QSPI/m-p/1051449#M6955</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;is it possible to use the external QSPI flash as program memory? If yes, how is the execution speed compared to internal memory?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 20 Aug 2020 09:57:41 GMT</pubDate>
    <dc:creator>peter_scheunert</dc:creator>
    <dc:date>2020-08-20T09:57:41Z</dc:date>
    <item>
      <title>S32K148 QSPI</title>
      <link>https://community.nxp.com/t5/S32K/S32K148-QSPI/m-p/1051449#M6955</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;is it possible to use the external QSPI flash as program memory? If yes, how is the execution speed compared to internal memory?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Aug 2020 09:57:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K148-QSPI/m-p/1051449#M6955</guid>
      <dc:creator>peter_scheunert</dc:creator>
      <dc:date>2020-08-20T09:57:41Z</dc:date>
    </item>
    <item>
      <title>Re: S32K148 QSPI</title>
      <link>https://community.nxp.com/t5/S32K/S32K148-QSPI/m-p/1051450#M6956</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, yes it can. It even exist example code showing that:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/application-note/AN12193.pdf" title="https://www.nxp.com/docs/en/application-note/AN12193.pdf"&gt;https://www.nxp.com/docs/en/application-note/AN12193.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However the device cannot boot from QuadSPI memory.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Aug 2020 15:49:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K148-QSPI/m-p/1051450#M6956</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2020-08-21T15:49:34Z</dc:date>
    </item>
  </channel>
</rss>